Part Number: AM4376 My customer is investigating CRA for their current products. They are using variants of the AM4376. The part numbers they have used for this are below:
AM4376BZDNA100
AM4376BZDNA80
They have used the AM62A on newer projects…
Part Number: AM4376 Hello,
We are developing custom boards based on AM4376BZDND30S processor with IS34ML08G088-BLI NAND Flash. After successful OTP fusing with TI key, we try to boot the board using SD card with MLO, u-boot.img, fitImage.itb and rootfs…
Part Number: AM4376
Hello,
We are using the AM4376 processor on a Linux-based platform with a secure chip. We have almost completed the first phase of development and have initiated activities for penetration testing and product certification .
…
Part Number: AM4376 Hello,
Our product is based on the AM4376, with the SDK version V09x, 09.03.05.02 (Dec 13, 2024) . This SDK version is built on the Linux V6.1.119 kernel, and I have noticed that TI has made customized source code modifications…
Part Number: AM4376 Other Parts Discussed in Thread: AM4372 hello! My development board uses the am4376 core board, which has three network ports, two native network ports, and one PRU network port. Previously, based on SDK 04.03.00.05 (Linux kernel 4…
Part Number: AM4376 Tool/software: Posting on behalf of the customer.
We are performing certification testing with UL, during testing device suddenly stop working.
We check all the voltages, it was fine. After that We enabled the Linux Kernel Low…
Part Number: AM4376 Tool/software: We are using the Linux kernel timer, but we are facing a larger jitter issue, especially when the timer interval is low like 1ms. Is there any other timer in TI RT Linux which gives a low jitter? Or can anyone suggest…
Part Number: AM4376 Hello,
we are currently analysing secure boot for AM437x-HS. As secure boot is already in use in our company based with the AM57xx-HS SoC, we would like to ask if AM437x-HS and AM57xx-HS share the same secure boot hardware and processes…
Part Number: AM4376
On our TI-AM437x platform, the network bridge ( br0 ) setup causes a system crash. The device completely hangs the moment we create the bridge over the PRU interfaces. Please advise on how to resolve this lockup issue."
oot@am437x…