Part Number: AM4377 Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi @All,
I do have custom board with AM4377 and I wanted to flash my VxWorks bin file the device using Blackhawk XDS200 debug probe .
so , how to flash the my custom board…
Part Number: AM4377 Other Parts Discussed in Thread: AM4376 Hi Expert,
The customer used AM4376BZDND80 to develop products before, and wanted to switch to AM4377 due to material shortage
The customer wants to know if there is any modification required…
Part Number: AM4377 Tool/software: Hi,
I am maintaining a product based on the Sitara AM4377 (it is a TI-RTOS based product no Linaro), and I could not find information about the command line options of the:
ProcessorSDKSerialFlash
program, which…
Part Number: AM4377 Other Parts Discussed in Thread: AM62P , AM625 , AM623
This processor is taking approx 600mA while recording the video pls suggest processor which should take max 100mA during video recording., suggest a low power video recording…
Part Number: AM4377 Hello,
We have a custom board with an AM4377 HS processor whose firmware is written on an external flash memory.
To flash this memory we load a .out program via UART that will receive the firmware and write it into the flash…
Part Number: AM4377 Other Parts Discussed in Thread: AM62A7 , AM625 , AM623 This processor is taking approx 600mA while recording the video pls suggest processor which should take max 100mA during video recording.
Part Number: AM4377 After suggested updates of ccs 9.3 I am no more able to import projects, neither from archives neither from directories. I get "See details below... Import failed for project 'BK41A100' because its meta-data cannot be interpreted.…
Part Number: AM4377
Basically we are making an AI based trail camera, which will be capturing and recording the video on the basis of movement detection through PIR Sensor and further transmitting it to a web server through LTE.
Our application involves…
Part Number: AM4377 Other Parts Discussed in Thread: UNIFLASH , , DP83848K Hello,
I work on the same projekt mentioned in AM4377: QSPI-Flash for AM4377 and we still have the problem that sometimes the board doesn't boot.
I have measured DCLK and nCS…