Part Number: AM4377 Other Parts Discussed in Thread: AM62P , AM625 , AM623
This processor is taking approx 600mA while recording the video pls suggest processor which should take max 100mA during video recording., suggest a low power video recording…
Part Number: AM4377 After suggested updates of ccs 9.3 I am no more able to import projects, neither from archives neither from directories. I get "See details below... Import failed for project 'BK41A100' because its meta-data cannot be interpreted.…
Part Number: AM4377 Other Parts Discussed in Thread: AM62A7 , AM625 , AM623 This processor is taking approx 600mA while recording the video pls suggest processor which should take max 100mA during video recording.
Part Number: AM4377
Basically we are making an AI based trail camera, which will be capturing and recording the video on the basis of movement detection through PIR Sensor and further transmitting it to a web server through LTE.
Our application involves…
Part Number: AM4377 In the AM4377 data sheet, there is a WARMRSTn(nRESETIN_OUT)pin, but there is less description about this pin. Can this pin be configured as either an input or an output? And why? Thank you!
Part Number: AM4377 In the AM4377 product, does the RTC_XTALOUT terminal have the function of an internal clock, but anything else? Does the system still need this clock configuration after power up? Can it be removed? Thanks!
Part Number: AM4377 Hello,
I am working on a custom board using the AM4377, based on the IDK437x. I am using the SDK ti-processor-sdk-linux-rt-am437x-evm-08.02.00.24.
We have a RTC RV8803 installed on the bus I2C, at the address 0x65. When in u-boot…
Part Number: AM4377 Other Parts Discussed in Thread: FLASH-PROGRAMMER , TLV803
Hello,
we have designed a custom AM4377 board and we experience some problems with booting from the QSPI-Flash. The board itself runs fine with the XDS-debugger - we are…