Part Number: AM4377
Hello,
we are working on the Sitara AM4377 and use the eQEP module for an incremental encoder.
The QEPCTL Register is configured in the way, that the position counter shall be reset on every index event (PCRM = 0).
Now we face…
Other Parts Discussed in Thread: SYSCONFIG Hi Team,
In AM437x Sitara Processors datasheet (SPRS851E –JUNE 2014–REVISED JANUARY 2019), the signal “mmc0_sdcd” can be routed to pins A17, N24, or R25.
However, in SysConfig tool (version 1.6.0_1543 …
Part Number: AM4377 Other Parts Discussed in Thread: SEGGER Hello,
we are developing a board based on the AM437x and want to use Code Composer Studio to debug it with the Segger J-Link Plus Emulator. The AM4377 is officially supported by Segger ( https…
Part Number: AM4377 Other Parts Discussed in Thread: SYSCONFIG Hi experts,
my question is related to [Resolved] AM4376: GPMC and PRU Ethernet pinmux - Processors forum - Processors - TI E2E support forums .
Usage of GPMC in combination with already…
Hi Zhang,
Do you need to find a way to autoload the w5100s ko modules during system boot up? Thus no need to load manually with insmod/modprobe?
You can also embedded these w5100s ko modules in the kernel image, thus no need to autoload or manually…
Part Number: AM4377
Hi
We are developing firmware for a custom AM437x based board. We are not using the TI SDK, but rather the Linux based firmware is created using Buildroot and a standard kernel.
While upgrading our previous kernel 4.19.45 to…
Part Number: AM4377 Hello Champs, Hardware: own AM4377 board which is designed by referencing EVM board
Software: ti-processor-sdk-linux-am437x-evm-06.03.00.106-Linux-x86-Install DTS: am43xx_evm_defconfig and am437x-gp-vem.dts It prompted below error…
Part Number: AM4377 Hi,
SDK: PRU-ICSS-HSR-PRP-DAN-01.00.05.01-Linux-x86-Install.bin
Customer connect RTL8201F with PRU1 MII in his customize board and he want to add HSR to the system.
1.He need to change pinmux configuration because pins which…
Part Number: AM4377 Dear Champs,
My customer failed to boot their custom board using emmc1 when it was partitioned using GPT
When they changed the partition to MBR in emmc1, there is no issue to boot.
Could you please check their gpt partition…