Part Number: AM4379 The secure SDK was downloaded and everything builds. I followed the steps to produce the key provisioning in DEBUG mode: ./smpk.sh 0 0 ./smek./sh 0 0 ./otp_img.sh 0 1 1 otp_cfg_dbg.txt otp_img_v1.0 => this creates a otp_img_v1.0_cfg_dbg…
Part Number: AM4379 I've had the AM437X processor for a while, swapped my design for an "S" version of the processor and tried loading my original, working U-boot-spl. It doesn't seem to work. Are these processors not code compatible?
Part Number: AM4379 Other Parts Discussed in Thread: UNIFLASH Hi,
My Uniflash version is Uniflash_8.5.0. Does it support S34ML01G200TFI000 Nand flash?
Best regards,
Yuzhi
Part Number: AM4379 Other Parts Discussed in Thread: SYSCONFIG Hi,
I cannot write data through GPMC, the program is shown as below. Could you help me with it? Thanks in advance.
GPMC_Config_t GPMC_ConfigNorDefault = { /* SysConfig - ROM Code defaults…
Part Number: AM4379 Tool/software: Sitara
AM4379BZDNA100
1. Is it necessary to use blind, buried, via-in pad, or any other exotic vias for this 0.65mm pitch BGA?
2. Is a standard 5mil trace / 5 mil space the correct width and space for the fanout…
Part Number: AM4379 Other Parts Discussed in Thread: SYSBIOS , UNIFLASH Hi, All
Working on a QSPI bootloader project for AM4379 Cortex A.
Since I'm using CCS, I download "Sysbios_ind_sdk 02_01_03_02" from here for easy import. https://software-dl…
Part Number: AM4379 Other Parts Discussed in Thread: TMDSIDK437X Hi,
I am working on one application in which i neeed to simulate the end device ethernet response whenever source device MAC sends TX_ER signal to its Phy over RGMII. Assumption is that…
Part Number: AM4379 Other Parts Discussed in Thread: AM4378 , TPD4S012 Tool/software: Issue Title : RNDIS USB device mode does not work after being switched from USB host under USB0 OTG mode configuration
SDK version : Linux-rt-am437x-evm-06.03.00.106…
Part Number: AM4379 Other Parts Discussed in Thread: TPS65218 Hi,
Our kernel board is a total new design board which is based on our vender demo board. It has a booting error, the booting log is shown below.
The setup is booting form SD card on…