Part Number: AM5708 Hello, on some boards with the AM5708 processor, during initialization in about 90% of cases, the IPU M4 core crashes when attempting to write to the unicache register, for example HW_WR_REG32(0x55080000U + IPU_UNICACHE_MAINT, 0x00000010…
Part Number: AM5708 I am currently developing a system that uses the AM5708, and I would like to ask about the reset sequence.
Regarding the resetn/porz timing requirements described in Section 5.10.3 Power Supply Sequences of the AM5708 Data Sheet…
Part Number: AM5708 We are planning to capture HD video from a USB 3.0 UVC camera on AM5708, crop a specific region, convert it to a 360p video, then encode it in H.264 and stream it over Gigabit Ethernet via an RGMII interface. When reviewing the Release…
Part Number: AM5708 The AM5708 sometimes freezes at random times, sometimes after a few hours, sometimes after a few tens of hours, or sometimes after a few days.
When it freezes, I can't access the program via JTAG or other means.
The cause is unknown…
Part Number: AM5708 Tool/software: Hi ,
We have a custom board based on the TI AM5708 SoC, running TI Processor SDK Linux. We're in the process of upgrading from:
sdk linux-am57xx-evm-05.03.00.07 to sdk-linux-am57xx-evm-08.02.01.00.
We use GPIO4_8…
Part Number: AM5708 I'm developing using the AM5708.
I'm using kernel version 6.1.119, but I'm experiencing a kernel crash.
I've been investigating various options, but I can't figure out the cause.
Could it be a kernel version incompatibility?…
Part Number: AM5708 This is regarding AM5708 and DDR3L settings using the EMIF Tool: Register Configuration.
In Step 1, under System Details, I set "Max DRAM Operating Temperature" to <=105°C.
Then, in Step 3, under DDR Timings, I enter 1950ns up…
Part Number: AM5708
Tool/software:
I am configuring a system using DDR3.
To match the DDR3 impedance, I need to set the impedance of the single-ended and differential signals.
According to the AM5708 manual, I can set Imp80 to Imp34Ω by setting…
Part Number: AM5708 Other Parts Discussed in Thread: TUSB8042A , I'm debugging using a prototype custom board. The TUSB8042A's PWRCTL won't go high. (Polarity is set to high.) I'm connecting the AM5708's us1_drvvbus to the TUSB8042A's USB_VBUS.
The…