Part Number: AM5726
We use Git in our project with several developers working concurrently.
Contributes work with git as follows
branch from origin/master to a feature branch
When they are done, merging or rebasing the latest origin/master to their…
Part Number: AM5726
Hi Team,
Customer want to apply two PHY in AM5726, but these two PHYs share MDC and MDIO.
1. So my question is can these two PHYs be used at the same time? How to distinguish and call these two PHY interfaces in software?
2. Could…
Part Number: AM5726 In SPRUHZ6L it states:
NOTE: Only DSP_CLK3 clock is supported on this SoC. Upon boot time, sysboot15 set at '1' selects a DSP_CLK3 divided clock version for the DSP subsystem logic and bus interfaces. For SR1.1, sysboot15 must…
Part Number: AM5726 Hi,
I'm working on a program on the DSP2 core of the AM572x that uses the IPC packages from TI. I based the project off of the IPC examples provided in the SDK. The build occasionally fails, even when nothing has changed in the files…
Part Number: AM5726 Hello,
I'm working on a DSP program on the AM5726 where we're attempting to DMA data from a FIFO provided by an FPGA on the GMPC to L2 memory in the DSP. My understanding is that the SAM and FWID bits in the PaRAM options (and therefore…
Part Number: AM5726 Hi,
My customer has been doing tests in dual mac mode, related to the PPS signal. Following the guidelines provided in this link ( https://software-dl.ti.com/processor-sdk-linux/esd/docs/06_03_00_106/linux/Industrial_Protocols_PTP.html#generating…
Part Number: AM5726 Other Parts Discussed in Thread: TPS659037 I want to power an AN5726 without GPU, EVE and IVA. According to SLIU011F page 4
I must connect the unused power pins to 1.06 V. Do I need to use the high current SMPS4 in parallel with SMPS5…
Part Number: AM5726 This is a follow up a thread originally posted by Tsurumoto regarding Isolation using AM5726.
Original post: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/983524/am5726-isolation
The ISOCLK_STATUS bit…
Part Number: AM5726
Hello,
I am working on an application where, after some initial setup occurs at boot, I want to prevent the DSP(s) from being able to access all but a small section of DDR memory. It seems like this might be possible using either…