Josue Zamitiz-Ayala said: I apologize Hanmant, but what you are doing is not supported by TI at this moment, please reach out to Wind River or the Open source community for further support.
Hi,
Jonathan Cormier said: Is there a SDK 10 in progress?
An SDK 10 won't be released,We will move straight on to SDK 11 after SDK 9.3.
Jonathan Cormier said: What is it's expected release date.
SDK 9.3 will be released in December 2024, while…
Part Number: AM5728 Tool/software: My AM5728 based board typically boots fine from mmcblk1p1 which is formatted as FAT. The FAT partition contains MLO, u-boot.img, device trees and Linux kernel. However, my board will occasionally fail to boot after u…
Part Number: AM5728 Tool/software: Hello, expert We used AM5728 bare metal dual network port mode, but the port fifo mode was configured as normal mode before, not DUA MAC mode. Is there any risk when using this configuration?
Thank you very much
Ha…
Part Number: AM5728 Tool/software: Hi All,
I have a question regarding VIDEO OUT / IN. What is the maximum allowable difference in the length of the following signal lines? If we can tolerate about 50mm, the board pattern will be greatly helped. Video…
Hi Fabiana Jaimes , On PC the gstreamer version is - GStreamer 1.24.2
On 6.03 Linux SDK for AM5728, version is GStreamer 1.14.4
But clearly, the issue seems to be with IVAHD h264 decoder!
Basically, I want to use IVAHD core for video encoding and decoding…
Part Number: AM5728 Tool/software: Hi,
Please give me the gel file of am5728 custom board . we are change 2gb DDR3 (EMIF1 & EMIF2) to 1gb (EMIF1) .
my gel file is
//#################################################### //AM572x GP EVM GEL
StartUp…
Part Number: AM5728
Tool/software:
Hi,
We are not able to boot into linux with AM5728 on our custom board (OS Release: 5.10 kernel PD23.1.1). After u-boot it was getting stuck at Starting kernel. Hence I enabled earlyprintk and was able to obtain logs…
Hi Vishal,
I am not familiar with the IVA-HD CODEC and am not sure about how to use CCS to monitor the decoder. According to the documentation ( here ), ducatih264enc is the hardware encoder, so by specifying this in the pipeline you are using the IVA-HD…