Part Number: AM5748
Hi TI Team,
We are using am5748 device, the GMAC support IEEE 1588 V2,
does Eth PHY also required to support IEEE 1588 V2 for time sync ?
presenlty we are using KSZ9031RNXIC Eth PHY that doesn't support IEEE 1588 V2.
Regards,
S…
Part Number: AM5748 Hi ,
I'am running RTOS MCASP audio example code in DSP core for AM5748 Custom board when I'm running this example using JTAG . we are seeing these prints below.
-------------------------------------------------------…
Part Number: AM5748 Hello,
We are using AM5748 in one of our design.
We are interfacing two Artix FPGA and one Spartan FPGA to the GPMC of the Sitara processor AM5748. Would like to know whether we need to provide a buffer at the output of AM5748 for…
Hello Arun,
This is not supported by our SW offering. When running Linux, you would have to use both cores of the A15.
For more information about bare metal support, also see the CSL library in RTOS SDK .
Part Number: AM5748 Other Parts Discussed in Thread: TUSB320 , , TPS2051B
We are using usb with am5748. We run USB2.0 over USB-C using TUSB320. PMIC is not involved in Vbus detection.
The Vbus detection was suggested and reviewed by TI some time ago.
…
Part Number: AM5748 Hi TI Team,
We are using am5748 device with PDK ( 08.02.01.00 ) u-boot and kernel,
we want to know that this PDK u-boot support UEFI boot, if yes then please provide procedure to enable that.
Regards,
Snehal
Part Number: AM5748
Hi,
I am working on DSP programming using an AM57x based SoM. Following the sdk documentation, I was able to establish the IPC communication between the DSP & ARM_15.
In the RTOS_template_app,
How can I turn ON/turn OFF a GPIO…
Part Number: AM5748 Hi,
I am trying to implement a socket programing that would communicate with the server of ip address 192.168.9.102.I am not facing any trouble with the code as it is not causing as crash.But i am not not able to see any packet transferred…
Christian Leeb said: We suspect that with the standard device tree settings the DWC3 controller is not properly configured. (evidence is that we have RNDIS running with VxWorks on a am43x platform (has the same dwc3 controller) and do not see this issue…