Part Number: AM620-Q1 Other Parts Discussed in Thread: AM620 Tool/software: We are using AM620-Q1 for programming and would like to leave the following question: 1. Is the PRUSS core in AM620 able to do BLDC motor control and the following resources are…
Part Number: AM620-Q1
Tool/software:
Hi all, Good day to all. Currently, we had mounted to our DUT AM6204 A SGFHIAMCRQ1 AM6204 B SGFHIAMCRQ1 We found out that there some issue on the SW flashing on our board after using the B -type AM6204 B SGFHIAMCRQ1 . Based…
Part Number: AM620-Q1 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Dear Champs,
we are looking into key writing process during production for AM6204. The key writer application outputs logs on main_UART0.
We do not have access to main_UART0…
Part Number: AM620-Q1 Tool/software: We need to manually reboot the board after some interrupt is hit can you please let us know what all register need to be considering for
completely rebooting the board. But, when I have configured the register as…
Part Number: AM620-Q1 Tool/software: Dear Expert
Do we have any way (or sample code) to reset MCUSS from main domain LInux A53 Core?
Because I know we have some way with FFI, MCUSS can reset main domain A Core, how about reverse case?
Thank You.
Gib…
Part Number: AM620-Q1 Tool/software: I have a question related to the architecture design of our new project:
Setting EPWM_ETSEL[SOCASEL] of ePWM to PRD_eq (010) via M4F (red box below). -- Is it possible to generate SOCA pulse on IO port of PWM_SOCA…
Part Number: AM620-Q1 Tool/software: Hi,
The communication between ARM and FPGA uses GPMC interface.
In the data manual (pin connection requirements on page 88), it is mentioned that these signals need to be pulled up and down externally,
but more detailed…
Part Number: AM620-Q1 Tool/software: hi :
we wish to know how to operator the mcu(M4 core) and soc(A53) software warm reset with each other.
refer to 《spruiv7b.pdf》- 6.3.5.2.3 SW_MAIN_WARMRSTz Reset and 6.3.5.2.4 MCU_RESETz Reset, i see these way but…
Part Number: AM620-Q1 Tool/software: Hello, In the AM620-Q1 data manual, it is recommended that the voltage of VDDA_1P8_CSIRX0 be 1.8V. If a MIPI camera with 1.1V or 1.2V is connected, does it require level conversion? At the same time, CSIRX0 is compatible…
Part Number: AM620-Q1 Tool/software: hi :
we wish to know how to operator the mcu(M4 core) and soc(A53) software warm reset with each other.
refer to 《spruiv7b.pdf》- 6.3.5.2.3 SW_MAIN_WARMRSTz Reset and 6.3.5.2.4 MCU_RESETz Reset, i see these way but…