Part Number: AM62P Tool/software: Hi,
We are designing our hardware around AM62P SoC and have started developing software desig as well. We need SoM based on AM62P
Please let us know the availability of chip, stability and life time of AM62P. Do help…
Part Number: AM62P Tool/software: Hello
I'm thinking about the requirements and learning possibilities, to design a Board with the AM62P.
Never did DDR4 routing before. What is the best starting point?
Also, is it feasible to design such a Board…
Part Number: AM62P Tool/software: Hi Expert,
From datasheet, I can see we can support 3840*2160 display, but I am not sure there is max width restriction or not. So I want double check with you, can we support 4270*937?
BR,
Biao
Part Number: AM62P-Q1
Tool/software:
Hi,
We are starting a new project, and we are using the AM62P-Q1 Processor. We noted on the schematics of the AM62 SKEVM the usage of the 3 terminal capacitors.
We have a few questions about their connection.
1. what…
Hi Suren,
Suren Porwar said: Just for my understanding glcolorconvert can’t be used for your usecase due to Weston/wayland dependency?
Yes. Best regards.
Hi Jhon,
The Linux SDK is designed to enable as many peripherals and cores as possible on the TI EVM. From there, we can start disabling/removing unused things and reducing the clock speed of some of these peripherals. For any unused cores, you can refer…
naman kumar said: 2.After configuring DevAddr = 0x12 and using API PMICApp_setGPIOPins() to change GPIO1 and GPIO2 as GPIO, I am able to access watch dog registers over I2C1.
Yes, this behavior is correct.
Hi Board designers,
The current circuit diagram is as shown in ② , and if there are no issues with this, I would like to proceed as is.
We have updated or will be updating the pin connectivity requirements to allow the unused open drain I2C interface to…
Part Number: SK-AM62P-LP Tool/software: Hi,
I am using the SK-AM62P-LP board with PSDK version 09.02.01.10 and MCU+SDK version 09.02.01.08. I have a TI dual-channel display with a resolution of 1920x1200.
Weston service works fine in both SD card and…
Hi Patrick.
Could you let me know what changes you have made in the DPL layer to enable the SMP mode? I am not sure whether there is any issues from the CCS as the SMP mode is not by default supported by the SDK, so I want to make sure nothing's missed…