Part Number: SK-AM62P-LP Tool/software: Hi,
I am using the SK-AM62P-LP board and attempting to download the latest version of the Processor SDK (PSDK). The total file size is 3.6 GB, but the download consistently fails after reaching 3.2 GB, leaving…
Hi,
Krunal Bhargav34 said: our EVM do not support BT656 and we don't have any SW drivers or documents that show how to enable BT656.
As mentioned earlier, we currently do not have software support for YUV data format.
Part Number: SK-AM62P-LP Tool/software: Hi I was adjusting my device tree to receive a GNSS communication through UART5, I've configured my device tree as shown bellow
diff --git a/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts b/arch/arm64/boot/dts/ti…
Part Number: AM62P Tool/software: Hi I can see the Gfx bench mentioned here https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/10_00_07_04/exports/docs/devices/AM62X/linux/Linux_Performance_Guide.html#graphics-sgx-rgx-driver For evaluation, I am using…
Hello James,
James Pan said: The built of the kernel is succeed. But the Installation of new kernel is failed.
Can you share a list of the .deb that resulted after the successful build of the kernel? (i.e. ls -la in the ~work directory).
Also, have you…
Hariraj,
Hariraj Vijayakumar said: steps to flash Linux in eMMC instead of sdcard
Please see here...
https://dev.ti.com/tirex/explore/node?node=A__AXEeWNLEW2jak3KzsCN3BA__AM62P-ACADEMY__fp5YxRM__LATEST
Regards, Andreas
Part Number: SK-AM62P-LP Other Parts Discussed in Thread: AM62P Tool/software: I've created a mcu_uart0 node as shown bellow
/ {
aliases {
serial1 = &mcu_uart0 ;
};
};
&mcu_uart0 {
status = "okay" ;
pinctrl-names =…
HI Board designers,
Depending on the use case TPS65224 can be used with AM62A7 / AM62A7-Q1 / AM62A3 / AM62A3-Q1 processor family.
Please refer below for queries related to operation of PMIC with 5V input
(+) TPS65224-Q1: PMIC operation with 5V operation…
Part Number: AM62P-Q1 Other Parts Discussed in Thread: AM62P Tool/software: Please ask if there is am62p emmc sbl startup tutorial。At present, we do not know which file is used, and the address of the file is burned
version:10.00.0014
please help…