Part Number: AM62X-PET-CALC Hi TI
As the spec listed in PMIC I2C side , SCL low time must longer than 1.3us when in fast mode.
But according the test result , the low time is 1.26us, whether can be modify in 6202 side to increase the SCL low time?
If…
Part Number: AM62X-PET-CALC HI TI expert
In the AM62x_TRM, mentioned support JESD84-B51 spec, but also list the High Speed SDR seems only can support under VCCQ = 1.8V.
My query is , when both VCCQ and VCC is connect to 3.3v, Whether high speed DDR can…
Part Number: AM62X-PET-CALC Other Parts Discussed in Thread: SYSCONFIG Hi TI
Currently we face a GPIO can't be controlled issue in bios.
Can you help whether the MCU_GPIO1/7/19/20 can be used ? And why we can't output high at these four ports? …
Part Number: AM62X-PET-CALC Hi TI Expert
As the snapshot show (Sprad06, chapter 2.7), the vpp power rail seens must enable for LPDDR4 used, if yes it may conflict with VPP power rail defination in AM62x Datasheet.
BR Jingcheng
Part Number: AM62X-PET-CALC Hi TI
For the LPDDR4 length matching view, I want know the max length skew of SOC package internal.
Can you provide this part info for layout design ? Preferd file tiye is .ppd and .txt .
BR Jingcheng
Part Number: AM62X-PET-CALC HI TI expert
Is there any update about the CAN port in AM6204?
Delete the MCU domain CAN , only reserved the MAIN domain ?
BR Jingcheng
Part Number: AM62X-PET-CALC Attached the SOC part and PMIC related schematic info.
Please help review the below item with high priority:
1.boot mode related configuration.
2.system control related signal.
3.Power consumption essessment info need help…