Other Parts Discussed in Thread: TMDS64EVM , SK-AM64B Hi TI Experts,
I have the below queries on using the SERDES in my design.
1. Supported Interfaces
2. Implementation Reference for PCIe
3. Implementation Reference for USB3.0
4. Can i use PCIe and USB3.0…
Other Parts Discussed in Thread: TMDS64EVM , SK-AM64B Hi TI Experts,
I have the below queries regarding the selection of evaluation module. could somebody highlight the key differences between the various AM64x evaluation modules ?
TMDS64GPEVM
SK-AM64 …
Other Parts Discussed in Thread: TMDS64EVM Hi Board designers,
Refer FAQs listed below related to custom board design for AM64x family of processors, that could be used along with other available design collaterals.
Sl no
Domain
Topic
Link
1
Links…
Part Number: AM6442 Other Parts Discussed in Thread: AM6412 , AM6422 , , AM2434
Hi TI Experts,
I have the below queries regarding the I2C interface:
Need information on the number of I2C interfaces available
Termination of I2C interfaces when used as I2C…
Part Number: AM6441 Other Parts Discussed in Thread: AM6442 We've received 25 units of our 2nd rev PCA with the AM6442 SR2.0 installed, including the various features recommended in the TI app note regarding how to make a PCB compatible with both SR1 and…
Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
Hi TI Experts,
I have the below queries regarding the crystal selection.
Recommended crystal frequency for MCU_OSC0
Do you have recommended part numbers for Crystal?
Can you help check if NX2016SA…
Grant Edwards said: Is it the same cable that's used to connect two EVM boards?
Yes
Grant Edwards said: Have any of the EVM clock selection resistors (circled on p30 of the EVM schematic) been moved/changed?
Not getting what you are looking for here…
Part Number: AM6441 I'm confused with all the different versions of the AM64x... Which configurations (e.g. AM6441BSEF, BSFG, BSEG, BSDG...) will support native HSR/PRP offloading in the PRU-ICSSG?
Thanks :)
Part Number: AM6441 Hello,
I'm currently investigating on how to use the different cores of the AM64xx between real time and non real time processing. All cores should access to the Ethernet part with different priorities in both direction (Rx/Tx…
Part Number: AM6442 Other Parts Discussed in Thread: TPS65220 , TPS65219 , , AM6411 , AM6422 , AM6412 , AM6421 , AM6441
Hi TI Experts,
Can you provide a List of collaterals that can be referred when starting a custom board hardware design.