Part Number: AM6526 Hi Team,
One of my customer is asking a question about the DDR50 operating frequency. In the datasheet, table 7-62 MMCi - DDR50, 1.8-V/3.3-V High-Speed DDR Switching Characteristics, it indicates that the MMCi_CLK MAX is 40MHz. The…
Part Number: AM6526 This question deals with the following Literature: https://www.ti.com/lit/an/spraar7i/spraar7i.pdf
Page 9:
“Maintain constant trace width after the SoC BGA escape to avoid impedance mismatches in the transmission lines.”
This…
Part Number: AM6526 Hi,
I have two SD cards with this partition table
Device Boot Start End Sectors Size Id Type /dev/mmcblk0p1 * 8192 212991 204800 100M c W95 FAT32 (LBA) /dev/mmcblk0p2 212992 278527 65536 32M c W95 FAT32 (LBA) /dev/mmcblk0p3 278528…
Part Number: AM6526 Hi:
I want to know if PTP and HSR/PRP is supported on SDK Linux for AM65X 08_01_00?I only find these feature on AM3X and Am5X
Thanks
Part Number: AM6526 Hi all,
differences seems to related to kind of clustering two A53 cores:
I need some more background:
What does this exactly mean ?
What influence does this have on application performance ?
Part Number: AM6526
Hi TI Experts.
I have some questions.
I went over AM65X IDK Board.
1. am65x really needs to have ECC memory mandatorily?
2. I want to put only 1GB or 2GB Memory without ecc memory, not like IDK Board. Is it possible?…
Part Number: AM6526 Other Parts Discussed in Thread: TMS570LC4357 , , HALCOGEN Does the TI SITARA AM6526 have inbuilt capability of TMS570LC4357 , like ECC RAM ,lockstep processing and all other functional requirements for SIL3 certification.
We are looking…
Part Number: AM6526 Other Parts Discussed in Thread: UNIFLASH , MSP-FET Tool/software: Code Composer Studio Hi,
The customer has developed their own board with AM6526.
- Is there any tool or firmware for writing Q SPI Flash ?
- Can UniFlash…
Part Number: AM6526 Hi Team,
One of my customer has a few questions about PCIe and want to change the PCIe settings for the best signal integrity.
They want to change the de-emphasis between 3.5dB and 6dB on the TX preset to confirm the best signal…