Part Number: AM6528 Other Parts Discussed in Thread: AM2434 Dears sirs,
we are evaluating if it is possible to implement on the same chip both:
an EtherCAT master for a local network
an EtherCAT slave toward a higher level EtherCAT network
…
Part Number: AM6528 Hi Team,
Could you please help us to check the customer's issue. I have shared the full details of inquiry below.
When display is kept idle for 20 minutes/ timeout happens, below crash is observed.
Below are the hardware and…
Part Number: AM6528 Hi,
still using processor_sdk_rtos_am65xx_07_01_00_14, I refer also to the
Promiscuous Mode on AM65xx - thread
The ICSS EMAC loopback application (without DDR) with the promiscuous workaround given in the above link is working…
Part Number: AM6528 Hi,
I'm still using processor_sdk_rtos_am65xx_07_01_00_14.
I have some trouble get the SBL running, which runs fine on IDK with SR2.0 but stalls on a target with SR1.0. It seems to be that the MCU crashes while accessing a pointer…
Part Number: AM6528
Customer needs two ethernet port, as there is only one external port of CPSW on AM65xx, so use one PRU ethernet as second port.
Question:
Can use one MDIO port to control the two ethernet port on CPSW and PRU? if yes, would…
Part Number: AM6528 My customers want to build and use their u-boot image.
I found that: you will need to copy the all the boot images (MLO and u-boot.img for 32-bit platforms, tiboot3.bin, sysfw.itb, tispl.bin, u-boot.img for K3 based platforms) files…
Part Number: AM6528 Is secure boot feature on AM652x available for catalog / mass market customers?
How to request for access to secure boot documents?