Part Number: AM67 Hi Team,
The customer is currently using the marvell_CN9130 series but is concern that the competitor product may be EOL, so customer would like to know whether the AM67 series support PQC?
Does AM67X support PQC (Post-Quantum Cryptography…
Part Number: AM67
Dear AM67 Support Team,
I hope this message finds you well.
We are currently evaluating the TI AM67 platform for an upcoming project and would like to confirm whether it supports the following features:
Linux-based operation…
Part Number: AM67 Tool/software: I am currently performing DDR analysis on the AM6754AKGHIAMWR and have downloaded j722s.ibs.
The models in this file include, for example,
"lpddr4_ocd_40p_40n_lt"
"lpddr4_ocd_40p_40n_ht"
But when should I choose…
Part Number: AM67 Tool/software: Hi all,
I used the AM67SDK 10/11, config mcan CANFD,
ip link set can0 type can bitrate 100000 dbitrate 500000 sample-point 0.8 dsample-point 0.75 fd on
ifconfig can0 up
ip link set can0 type can bitrate 100000…
Part Number: AM67 Other Parts Discussed in Thread: TUSB321 , Tool/software: Hi Sirs
We find resistor in TUSB321 id pin in AM67 reference design is 10K pull high.
However, TUSB321 id pin is suggest to 200K pull high in TUSB321 datasheet
Do you know…
Part Number: PROCESSOR-SDK-AM67 Other Parts Discussed in Thread: AM67 Tool/software: Hello,
Is there a Linux kernel performance guide for AM67 like there are for AM62x devices?
Usually this seems to be provided as part of the SDK documentation but…
Part Number: AM67 Tool/software: Hi all,
I used am67 sdk 10.0.1in the AM67 EVM, when I test watchdog, it can't reboot, how to test watchdog reboot in the AM67 EVM SDK?
Thanks
Part Number: AM67 Tool/software: Hi Sirs
Can AM67 support 3 independent displays as below?
1.
a. I ndependent LVDS-SL to one display by using OLDI0~OLDI3, CLK0
b. The other I ndependent LVDS-SL to one display by using OLDI4~OLDI7, CLK1
c. DSI…
Part Number: AM67 Tool/software: 1)Based on scopeshot, the swing is 400mV(remove 50 ohm )green color
the swing is 200mV(add 50 ohm ) Blue color
2)And based on internally discussing, the 50ohm external resistor to gnd is a requirement of the PCIe…
Part Number: AM67 Tool/software: Dear all,
am67 SDK 10.0.1.
root@~# gpioset 0 31=0 root@~# gpioset 0 31=1
I measure gpio0_31 voltage value, it is 3.3V
root@~# gpioget 0 31 1
when I readback gpio0_31, the read value is right, but I measure gpio0_31…