Part Number: AM67 Tool/software: Hi all,
When I Press ENTER to u-boot, run md 0x600000, gpio IN_DATA reg don't diaplay right value
when I run gpio status command, and run md 0x600000 command again, gpio IN_DATA reg diaplay right value
why gpio…
Part Number: PROCESSOR-SDK-AM67 Other Parts Discussed in Thread: AM67 Tool/software: Hi Expert,
Does AM67 have plans to support Android in the future?
Thanks
Daniel
Part Number: AM67 Tool/software: Hi Team,
The camera sensor module which we are planning to integrate with the AM67 has four signals HSYNC, VSYNC, MCK and NRST apart from the CSI data and clock signals. I couldn't find dedicated pins for the sync, mck…
Part Number: AM67 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Champs:
Where is the AM67 DDR tools?
This link shows nothing....
please fix it.
BR Rio
Part Number: AM67 Tool/software: Dear all,
I use am67 SDK 10.0.1, i config two NIC used rgmii0 and rgmii1, the eth0's MAC address is fixed, same as c0:d6:0a:f1:4f:xx, but eth1's MAC is random, why the eth1's MAC is not fixed? how to fixed it?
Tha…
Part Number: AM67 Hi team,
Is it possible to have 3 USB ports from AM67? I am thinking of using the two dedicated UBS ports and then 1 SERDES port as USB. Is this possible?
If yes, are there any caveats in doing this? Any challenges or limitations…
Part Number: AM67 Other Parts Discussed in Thread: SYSCONFIG Hi Experts,
My customer is asking about DDRSS config. My customer generates .dtsi file by enabling with below option.
The question is how customer can confirm the output file is expected…
Part Number: AM67 Hi AM67 Support Team, our customer wants to combine the two interfaces MMCSD1 and MMCSD2 into one 8-bit width bus. Is this possible with the AM67?
Thank you, Dave
Part Number: AM67 Tool/software: Hi all,
I used am67 sdk 10.0.1 u-boot 24.04, in the u-boot used usb host, when I reun usb start, it display:
starting USB... No working controllers found
how to used usb host in the uboot?
Thanks
the u-boot usb…