Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1204 , HI team,
My customer used AMC1204 in old project. They would like to upgrate to AMC1306. Do they need change anything? Including software and hardware.
Thanks!
Other Parts Discussed in Thread: AMC1306M25 , AMC1204 The schematic diagram is as follows:
After sampling with AMC1306M25 oscilloscope test motor U phase and V phase waveform is as follows:
You can see spikes in both phases;
Same program and…
Part Number: AMC1306M25 Hi Team,
Could you pls recommend suitable device of two-channel buffer for CLKIN and DOUT pin in AMC1306M25 device? Thanks.
Best,
Stanley
Part Number: AMC1306M25 Hi,
I would like to know,why the larger the OSR, the smaller the BANGWIDTH will be.
BANGWIDTH refers to the frequency of the input signal?
Thanks
ZT
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1204 , Dear Teams,
According to datasheet, the Vcm for AMC1306M25 (0.16 to AVDD-2.1V) is narrow than AMC1204's Vcm (-0.16 to AVDD). Also, the CMRR for AMC1306 95db is smaller than AMC1204's…
Part Number: AMC1306M25 Hi
I want to test F280049 SDFM with AMC1306M25 on a universal PCB board, I bought some SOIC-8 to dip
adapters but SOIC-8 dimensions are different to the ones described on AMC1306 data sheet.
I checked SOIC-8 package on internet…
Part Number: AMC1306M25 Hi all Our customer are looking for isolated ADC with following specs; -8 pin PKG(because there is the limitation on the customer's board.) -Reinforced isolation -Internal LDO So, it's like as the product which is AMC1306M25 with…
Part Number: AMC1306M25 Other Parts Discussed in Thread: TLC04 Good Afternoon
I am using an AMC1306M25 isolated amplifier, interfacing to a 4th order butterworth filter to generate an analogue output voltage. I am measuring a changing voltage between…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1336 Dear Teams,
My customer is using F280049's SDFM function. Do you have any suggested external SD modulator to match with F280049?
Customer requirement:
Vin range: 0-10V
Bit: 14-16bits…