Tony,
Please refer to the following resources for C6748 LCDK development.
LCDK Wiki:
http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_%28LCDK%29
The software for the LCDK is packaged inside C6BIOS SDK.
C6 BIOS SDK Download…
Amy,
I think you have made a good choice with C6748 device. It was originally designed as an audio processor.
To answer your question on EVM, I think that the new LCDK would be a good place to start. It has line in/out interface available. Information…
You will need to obtain the BIOS PSP (Platform Support Package) to obtain the peripheral drivers.
http://focus.ti.com/docs/toolsw/folders/print/biossw-c6748.html
Hi Peter,
NOR Writer:
1. Download & Install TMS320C6748 SYS/BIOS Software Development Kit from below link.
http://www.ti.com/tool/biossw-c6748
2. Please find the "NOR Writer" under tools directory.
Installation path: ..\c6sdk_02_00_00_00\tools…
Other Parts Discussed in Thread: BIOSSW-C6748 , STARTERWARE-C6DSP I am now using c6748 to send data frome emac, and there is no system like DSP/BIOS ,it is barely.
How to judge if the emac has send a package out? any useful register bit can be check…
Wing,
BSL library is only supported on the OMAPL138 EVM and is provided by Logic PD who manufactures the EVMs. You can do the same functions on LCDK using Starterware package. If you are looking for specific drivers the latest SYSBIOS PSP packgae supports…
Mark Duda,
Thanks for your post. I understand from your thread, you are working on TI OMAPL138 LCDK. Yes, It is possible for implementing of video or jpeg codec on OMAPL138 LCDK. You can use the available vpif interface in OMAPL138. And also refer the…
Other Parts Discussed in Thread: BIOSSW-C6748 Hello
I'm looking for a development kit for DSP C6746. Someone can help me ou advice me ?
My problem is the size of the BOOT ROM and if I can code inside...
Thanks,
Nicolas,
There seems to be a SATA BIOS 5.x driver provided as part of the C6748 BIOS 5.x PSP. Please look at the PSP section of the below link: http://www.ti.com/tool/biossw-c6748 Once you find the PSP the datasheet and user's guide should give more…