Part Number: BOOSTXL-CC1125 Other Parts Discussed in Thread: CC1125 Tool/software: Code Composer Studio Hi friends, I have faced so many difficulties when I tried to communicate using CC1125. Since I am beginner, I got support only from the queries which…
Have you referred to the associated Application Reports and Getting Started Guides?
SWRA520: www.ti.com/.../swra520.pdf
SWRU487: www.ti.com/.../swru487.pdf
SWRA493: www.ti.com/.../swra493.pdf
You can choose to load projects into CCS or the BOOSTXL…
Part Number: BOOSTXL-CC1125 Other Parts Discussed in Thread: CC1125 , CC1190 , CC1120 , CC1120EMK-420-470 , CC2511 I have 2 booster CC1125 eval boards. I am trying to go through exercise 5 in SmartRF Studio 7. When I set up the RX side the status button…
If you are able to, see if you find a converter cable between the connector used on BOOSTXL-CC1125 and SMA (or if you have a semirigid cable, try to solder one on) I'm not familiar with the booster pack details so I have never looked into the connector…
Part Number: BOOSTXL-CC1125 Hi,
I have 2xBOOSTXL-CC1125, and I would like to use both from the same PC through SmartRF Studio. However, SmartRF Studio recognizes only one module. Other tools, such as packet sniffer, recognize two devices. Clicking …
Other Parts Discussed in Thread: MSP430F5529 , BOOSTXL-CC1125 Hello,
I am trying to talk to the MSP430F5529 + BOOSTXL-CC1125 with the example software with a terminal emulator on Android (Windows works perfectly). Unfortunately I cannot find a terminal…
Part Number: BOOSTXL-CC1125 Other Parts Discussed in Thread: CC1125 Tool/software: Code Composer Studio Ok, so I have painfully followed all the procedures for setting up the Sigfox SDK with my launchpad and CC1125 boosterpack, and after 2 months of pestering…
Part Number: CC1125 Tool/software: In particular, CC1125EM-420-470-RD - for the 450 MHz band, but 890MHz would do.
It seems that the CC1125DK includes two (890MHz):
https://www.ti.com/tool/CC1125DK#tech-docs
But are they available separately?…
Part Number: BOOSTXL-CC1125 Other Parts Discussed in Thread: CC1125 , CC1310
Hello,
I'm willing to test the Sigfox network for an application here in Italy. Following TI's guidelines, I have obtained both the MSP430F5529 LaunchPad and the CC1125 BoosterPack…
I don't know for sure that it isn't entering SLEEP.
However, AIUI, after a power-up or manual reset, it should be in IDLE - so consumption 1.3mA typ.
So sending an SPWD strobe in that state should show a drop to 1uA max - and I'm not seeing that.…