Part Number: BOOSTXL-CC2650MA Tool/software: So I'm using the MODA as an independent device for all my tasks. I have done the necessary header modifications and I've also added my Sensor Controller Code and the code also works. But the problem is, the…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: CC2564C , CC2340R2 We want to add A2DP audio source functionality to our existing product.
We need to send microphone audio via Bluetooth to off-the-shelf bluetooth speakers. Connecting…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: LAUNCHXL-F280049C , CC2650 , LAUNCHXL-CC26X2R1 , SIMPLELINK-CC13X2-26X2-SDK I want to use the boostpack BOOSTXL-CC2650MA with LAUNCHXL-F280049C to achieve wireless communication between two…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: UNIFLASH Hi,
I am trying to load program 0 into the MSP4321R with it connected to the CC2650MA by following the instructions on this page: http://dev.ti.com/tirex/explore/node?devtools=BOOSTXL…
Part Number: BOOSTXL-CC2650MA Hi,
I am trying to flash program 0 into the MSP432P401R while connected to the CC2650MA by following the instructions on http://dev.ti.com/tirex/explore/node?devtools=BOOSTXL-CC2650MA&node=ABK4r-KkcNI2-Z79Tqd43A__FUz-xrs__LATEST…
Part Number: BOOSTXL-CC2650MA I've successfully ported the updated github version of the SPP_BLE_Server project to the BOOSTXL-CC2650MA, and essentially want the serial data attributes without the status or config attributes. My initial approach was to…
Part Number: EVM430-FR6047 Other Parts Discussed in Thread: BOOSTXL-CC2650MA , , CC2650 Hello Guys,
Good day.
Is BOOSTXL-CC2650MA compatible with EVM430-FR6047?
Our customer need Bluetooth 4 with the EVM module. If the CC2650 doesn't work, do you…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: SYSBIOS , CC2650 I am trying to run the simple_broadcaster_cc2650lp example except running with the BOOSTXL-CC2650MA connected to a XDS110 debug probe. (I have modified the project to define…
It looks like you are using serial boot loader to update your BOOSTXL-CC2650MA but fail. You might need to use Flash Programmer 2 and XDS110 Jtag connecting to BOOSTXL-CC2650MA to do mass erase and try again.
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: SYSBIOS Starting with the updated SPP_BLE_Server example from Github, I have two separate tasks I've added, one of which loops with a variable delay for Task_sleep() blocking it for a bit…