Hello experts,
I move the project from custom board to LAUNCHXL-CC1352R1 and connect to BOOSTXL-CC3120MOD.
The result is the some, sl_Start() hang on the begining of the call in _SlDrvDriverCBInit().
After that faultISR.
I see calls to _SemaphoreP_create…
Now I used CC3120MOD from BOOSTXL-CC3120MOD and connect it to a evaluarion board of same processor the custom hardware use.
Now I can connect the HOST_IRQ line and uart lines RX, TX, RTS, and CTS. Other lines for SPI kept open. Just HOST_SPI_CS with pullup…
Other Parts Discussed in Thread: CC3130 , CC3120MOD , BOOSTXL-CC3135 , CC3235MODSF Hello, i want to convert my analog signal from sensor with 18 bit ADC shown bellow.
but then i need to modulate is (18 levels) and trasnmit using filter mixers etc..
Is there…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: BOOSTXL-CC3120MOD Tool/software: Code Composer Studio Hello, I'm trying to write some code that will be able to program a Boostxl-cc3120MOD over UART using my launchpad. To do this I need to…
Hi Sarah,
1. I use CC3120BOOST and BOOSTXL-CC3120MOD.
2. One more thing.
I find out that when I use BOOSTXL-CC3120MOD with MSP-EXP430F5529LP and try to download the same code for debug - failed download code...
With CC3120BOOST no problem.
3. For my project…
Hello,
I recommend you use the schematic/BOM found in the BOOSTXL-CC3120 Hardware Design Files as reference. You can download this from the BOOSTXL-CC3120 TI page, or simply click here . The antenna that is used on this EVM is Taiyo Yuden's AH316M245001…
Hi Brian,
If you use the CC3120MOD this is already a certified design. The benefit of using the module is that the critical layout of the IC within the module is taken care of. If you then integrate our module within the final design using our integration…
Part Number: MSP-EXP430G2ET Other Parts Discussed in Thread: MSP-EXP430F5529LP , CC3100MODBOOST , BOOSTXL-CC3120MOD , CC3220SF-LAUNCHXL i like to connect MSP-EXP430G2ET to cloud via WiFi...if it is possible can u suggest me the steps or booster packs that…
Part Number: MSP-EXP430G2ET Other Parts Discussed in Thread: MSP-EXP430F5529LP , CC3100MODBOOST , BOOSTXL-CC3120MOD , CC3220SF-LAUNCHXL I like to upload sensor data to cloud, can i do it directly by adding booster pack to my MSP-EXP430G2ET .... if i can,…
Hi Nomo,
Perhaps the HW design of the CC3120MOD boosterpack could shed some light on your questions.
www.ti.com/.../BOOSTXL-CC3120MOD
1. Looking at the schematics of the CC3120MOD boosterpack, you can see that pins 48 and 49 are respectively connected…