Tuan,
Thanks for posting on the MD forum!
The DRV8332 is an older part, it was created before our more recent parts which incorporate things like 3xPWM control.
For example, a similar part that's newer and has 6x, 3x, or 1x PWM modes is the DRV8320…
HI Board designers
Refer below section for each processor family that includes links to key collaterals and FAQs that could be leveraged during custom board design and also while performing a self-review.
Recommended References for review and design…
Part Number: F29H850TU Other Parts Discussed in Thread: TPS37 , TPS650363-Q1 Hello experts!
I'm developing an application which requires performance level D and for this reason I need a second way to monitor the supply voltages of the MCU besides the…
My motor :
user_mtr1.h:
//! \file /solutions/universal_motorcontrol_lab/common/include/user_mtr1.h
//! \brief Contains the user related definitions
//! This file is used for each device includes F28002x, F28003x, F280013x,
//! F280015x…
Part Number: C2000WARE-MOTORCONTROL-SDK Other Parts Discussed in Thread: C2000WARE , BOOSTXL-DRV8323RS , DRV8323 , CSD88599Q5DC Hi team,
Here's an issue from the customer may need your help:
Environment is as follows:
power supply:12V/100A
Code…