Part Number: AMC0106M05 Hello , We can not get digital output on the evaluation board for the AMC0106 What we have tried to solve: 1) power supply: supply p3v3 external , put on r514 and r512 to supply internal 3.3 the analog voltage had 24 V connected…
Part Number: F29H850TU Other Parts Discussed in Thread: LAUNCHXL-F29H85X , DRV7308EVM , BP-AMC0106-LMG-MD , BOOSTXL-LMG2100-MD , LAUNCHXL-F2800137 , LAUNCHXL-F280049C , DRV7308 Hello, I am currently working on a project using the LAUNCHXL-F29H85X development…
We have not submitted our hardware to the email mentioned above, I am using default image downloaded from this link
https://dr-download.ti.com/software-development/software-development-kit-sdk/MD-1BUptXj3op/08.02.00.24/tisdk-default-image-am335x-evm…
Jim,
I just tried this on SK-AM62A, which has 4GB of DDR, using last-year's SDK v9.x U-Boot image. There was no issue accessing memory above the first 2GB.
First, you can confirm the memory map with U-Boots `bdinfo` command. You can see that the first…
Part Number: AM625 Other Parts Discussed in Thread: SYSCONFIG Hi all,
We have a custom AM6254 board with 4GB DDR. This board was running well the 4G DDR at 800MHz for a few months.
Recently we updated to the latest scarthgap revision of meta-ti (tag…
Hi Sanjay,
Thank you for your reply. My customer faces unwanted pop noise when enabling the reset although the external mute circcuit is implemented on the circuit. Do you see any causes of this pop noise and any ideas to remove it? I adviced him to…
Yes it is possible.
If there is network then you can always use tftpboot. If no network you can use UART to load the changed boot loader binaries to RAM. For example: Boot to u-boot prompt. Then on U-boot prompt enter command loady. You will see something…
Hi David, I just tried one way & this should be possible. If there is network then you can always use tftpboot. If no network you can use UART to load the changed boot loader binaries to RAM. For example: Boot to u-boot prompt. Then on U-boot prompt enter…
Hi Kevin,
I am awaiting your views on the above post.
My customer focused on the possible causes in the subsequent investigation. The details are as follows. - U-boot is written to eMMC to make eMMC boot. - Mounted memory is 512MB (2Gbit x16bit bus…