Other Parts Discussed in Thread: BQ24115 I've notice in the bq24115 data sheet that a Rin resistor is required for high power applications, but does not detail on exactly how this resistor should be placed. Only that it should be placed between the input…
Ryler,
Rev B is the release version of the bq24115 EVM and all of the documentation supporting this EVM support the version you have.
The EVM user guide can be found here: http://www.ti.com/lit/ug/sluu200a/sluu200a.pdf
The user's guide is on rev…
Other Parts Discussed in Thread: BQ24115 I am building a 3 cell lithium battery charger using the bq24115. I've used the typical setup with the following values.
R.sence=.1 ohm
R.set1= 10k ohm
R.set2= 5k ohm
V.in= 13V
V.out=11.9V
My problem…
Other Parts Discussed in Thread: BQ24115 Hello everybody,
I currently use BQ24115 product on my design.
I have validate almost 95% of functionalities ... but one functionality is not working.
When Charge is not enable, STAT1 is OFF
When Charge…
Hello Greg,
Unfortunately with switching devices you will lose the distinction of the battery state/fault condition information from the STAT2 pin.
I am not sure what you mean by the last two sentences. The BQ24115 will manage the CC and CV control…
Other Parts Discussed in Thread: BQ24115 , BQ2031 Hi,
Is there any reference designs using bq24115/105 with SLA batteries?it would be very helpful, if test reports are available.
-Ramesh
Part Number: BQ24105 Other Parts Discussed in Thread: BQ24115 , BQ24171 , , BQ24125 , BQ24172
A block diagram of the BQ24171, BQ24172, BQ24105, BQ24115, BQ24125 connection to the battery is shown below:
The charge current flowing across the resistances…
Part Number: MSP430G2553 Other Parts Discussed in Thread: BQ24115 Hello,
I was hoping for a schematic review of the use of the MSP430G2553 device in the linked schematic. Specifically if the reset button implementation is proper, the SBWTDIO/SBWTCK…
Part Number: BQ76925 Other Parts Discussed in Thread: BQ24115 , MSP430G2553 , TPS542951 Hello,
I was hoping for a review of my user of the BQ76925 in my schematic. It will be used in conjunction with the BQ24115 as can be seen in the schematic, it is…