Part Number: BQ24618 Other Parts Discussed in Thread: TPS65987D Question 1:
Is there a way to force both switches off in the BQ24618?
Question 2:
What happens to adapter and battery switch control when CE pin is held low? As a corollary, what happens…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS65982 , BQ24618 , , LM3489 , USB-CTM-MINIDK-EVM Tablet on UFP USB-C connector using TPS65982/7 for PD control.
Wall brick barrel connector and dock battery as power sources in addition to Tablet as…
Part Number: BQ2970 Other Parts Discussed in Thread: BQ24618 Hello, I want to use the BQ29700 device together with the BQ24618 charging controller.
So now my main question is if these components will works fine together?
Because the BQ24618 has still…
Part Number: BQ24618 Hi,
We are using below part in the Design.
Part.No: BQ24618
1) We are powering the IC with 5V adapter Input. We would like to know the voltage on REGN Pin for this input voltage
2) what is the voltage of "ACN-6V"(Net Shown in the…
Hi Ruben,
We have not heard form you in a while, and assume you were able to solve your issue. Please feel free to re-open this thread if any issues exist.
Part Number: BQ24618 Hi,
This problem was related to noise on the SRN and SRP battery current sense resister traces back to the 24618 chip. Although I paired the traces, they were routed too close to the high-current switching lines. In addition, the…
Hello Nasrin,
Nasrin Enayatzadeh said: I'm studying BQ24618 more; I want to make sure using one Cell, 3.7V battery is suitable for this IC.
Yes, BQ24618 should be able to support battery charge voltages between 2.1V-26V.
Best Regards,
Christian. …
Hi,
We haven’t heard back from you for a while, the thread is considered solved and closed.
Thanks!
Please click "This Resolved my issue" button if this post answer your question.