Part Number: C2000-F28004X-POWER-EST-CALC Hello,
The C2000-F28004X-POWER-EST-CALC tools has been unavailable for download the past few days due to maintenance.
Sorry! We're currently doing site maintenance. (ti.com)
F280049CPZQR: C2000-F28004X-POWER…
Hi Daisuke-san,
Daisuke Maeda said: Was a heatsink used for the AM62x on the board used for measurements in the application note?
There was not one used. Instead a Thermal Flow System, TFS.
Daisuke Maeda said: What is the airflow (m/s) under temperature…
Part Number: TMS320F280038C-Q1 Hi,
there is a power estimation tool available for F28004x -> https://www.ti.com/tool/C2000-F28004X-POWER-EST-CALC
Is there something available or planned for F28003x ?
Thanks and best regards,
Gregor
Part Number: LM25183-LM25184DESIGN-CALC Hi Team,
Our customer is evaluating LM2584 and use design calculator below,
7230.LM(2)518x PSR flyback converter quickstart tool revB.xlsx
Customer would like to understand the chart below, is it means switching…
Part Number: ZIGBEE-POWER-CALC TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI…
Part Number: C2000-F28004X-POWER-EST-CALC Hi
I am running a real time application and need to update the ePWM comparator values EPwm1Regs.CMPA.bit.CMPA and EPwm 1 Regs .CMP B .bit.CMP B for the same value (i do it for 3 modules at a time). I was wandering if…
Part Number: AM62X-PET-CALC Hi TI
I use the Power consumption assessment sheet provided by TI.
When i select HS200 +Utilization 100%, but 0mA SOC_DVDD1V8 current result is show which not make sense, as the SOC_DVDD1V8 is connect to VDDSHV4 port which…
Part Number: AM62X-PET-CALC Hi TI Expert
As the snapshot show (Sprad06, chapter 2.7), the vpp power rail seens must enable for LPDDR4 used, if yes it may conflict with VPP power rail defination in AM62x Datasheet.
BR Jingcheng
Part Number: LM5149-LM25149DESIGN-CALC One customer requested that LM5149-LM25149DESIGN-CALC add notice or cell's limitation or alert if power loss are extremely increased.
When output current and other specs enter severe spec, power loss are extremely…
Part Number: AM62X-PET-CALC Hi TI
In the power estimation tool, how to selec the mode column list as below?what's the represent meaning of every item?when i used this port as GPIO which one can i select?
BR JINGCHENG