XER0904_Page1_TIBlock.pdf Hello Sreenivasa, I am Michael, Tom's colleague also working on this project. Here is a PDF of the TI block, the USB and JTag connections are shown in the upper right hand corner If you need to see another part of the schematic…
Part Number: TPS2812 sluu139.pdf
Figure 1
How are the RC parameters of the two snubber circuits (R20, C16, R21, C17) of the push-pull converter in Figure 1 taken? How to calculate the power consumption of R in the snubber circuit?
In addition…
Hi Toshiki,
toshiki kouzai said: Is there a pinmux table available for MMC2? I searched through the TRM but was unable to find it. Is it not documented there?
The pinmux table for MMC2 interface is shown in the J722S datasheet. I am attaching the…
Hi,
You would have to put the pin group into &wkup_pmx2 instead of &wkup_pmx0.
Reason : - The base address of the &wkup_pmx2 when added with the 0x064 (for wkup_gpio0_3) result in the register address of the wkup_gpio0_3 which is 0x4301C0CC according…
Hi Gautham,
You can refer to the below datasheet for the pin configuration. You can set the UART2 to set its TX line to pin AA24 and its RX line to pin AA26.
J721E_Datasheet.pdf
Best Regards
Gokul Praveen
Hi Manikandan,
It is present in the below datasheet :
J784S4_Datasheet.pdf
Section having the timing data(HS400 mode) which is basically HS200 DDR.
Regards
Gokul
Part Number: AM62A7-Q1 Other Parts Discussed in Thread: SK-AM62A-LP , AM62A7 Tool/software: Dear Forum,
I have found a contradiction between AM62A data sheet:
According to section 7.10.2.2.1 Power-Up Sequencing in CPU datasheet, notes 10 and 11, …
Part Number: SK-AM62-LP Other Parts Discussed in Thread: AM62A7 Tool/software: Hello Team
I have one SK AM62LP evm board with ID ASSY PROC124E2A where I want to use one of the expansion pin as GPIO , where I can connect LED and test . Here I am trying…
Part Number: TDA4AH-Q1 Other Parts Discussed in Thread: TDA4VH Tool/software: New hardware design for
TDA4AH88TGAALYRQ1
TDA4VH, TDA4AH, TDA4VP, TDA4AP series
I am starting a new design for this Ti SOC.
I have a few questions.
For the DDR4…