Hi Jan,
This feature exists currently in the Connected Audio Framework (CAF).
This software uses the C5535 DSP (or similar family members) basically as a USB sound card.
The USB software is written and open source.
There are two places in the…
Kaka,
Please check out the Connected Audio Framework (CAF) www.ti.com/.../c55x-audioframework which provides a way to funnel audio via USB.
Hope this helps.
Lali
Colin,
There is the Connected Audio Framwork (CAF) www.ti.com/.../c55x-audioframework that can do USB audio. However, the examples are for the C5535 and C5515 when you download the package. You can make some changes to the CSL layer and be able to…
Hi Akash,
You can download it from here:
http://processors.wiki.ti.com/index.php/C5000_Connected_Audio_Framework#Download
http://www.ti.com/tool/c55x-audioframework
I'm not sure that the stereo record works seamlessly, but it can be enabled. See…
Randhir,
I'm unaware of any migration guide for the TAS1020B to the C5535. However, please take a look at the Connected Audio Framework www.ti.com/.../C55X-AUDIOFRAMEWORK on using the C5535 as a USB audio device.
Please also see processors.wiki…
Part Number: TMS320C5515 Other Parts Discussed in Thread: C55X-AUDIOFRAMEWORK Hi there,
My equipment:
Windows: 7, 64bit
CSS 5.5.0.00077
Board: TMS320C5515EVM
C55X-AUDIOFRAMEWORK: v02.00.02.04
Headset: Logitech with 3.5mm jacks for earphones…
Diego:
Have you tried looking at www.ti.com/.../c55x-audioframework
It might be a good starting point to get you up to speed with the ezdsp for the 5535.
Hopefully, that helps.
Alvis,
As a starting point, could you please take a look at the C55x product page? There are several flavors of the device available.
http://www.ti.com/lsds/ti/processors/dsp/c5000_dsp/c55x/overview.page
We typically recommend the http://www.ti…
Part Number: TMS320C5535 Hello,
I downloaded C55x connected audio framework from http://www.ti.com/tool/c55x-audioframework (v.02.00.02.04, date 15/5/2013). It seems that the project is made for ccsv5 but I imported it in ccsv7.4.0.00015, installed…
Hi Marc,
I would assign one AIC3204 as master (drives BCLK and WCLK) and then slave the other AIC3204 and the 2 C55xx devices to that single I2S master.
For going across the border, the AIC3204 is capable of deriving its MCLK from the BCLK pin.
Assuming…