Part Number: C6000-CGT Other Parts Discussed in Thread: TMS320C6678 , SYSBIOS Tool/software: When I build project containing SYS/BIOS with new CGT 8.5.0.LTS, I got an error:
"C:/TI/bios_6_83_00_18/packages/ti/posix/ccs/time.h", line 103: error #102…
Part Number: C6000-CGT Tool/software: I am looking for the C6000 V8.1 compiler to use with an existing project. The online resources only have version 8.3.1. Is it possible to get a v8.1 download.
Part Number: C6000-CGT Tool/software: We are using Code Composer Studio v6.1.3 and attempting to run the XDS 560 Pro Trace emulator. The error is "license cannot be acquired." I have ti_emupack_setup_5.1.636.0.exe which we used in the past but this errors…
Part Number: C6000-CGT Tool/software: Hello, In the following example, the struct does not contain the expected values after initialization. The 10th element is not correctly initialized. If I use float instead of double for e.g. var5, then the program…
Part Number: C6000-CGT
Hi,
I'm facing an issue with dis6x.exe, when I try to run disassembler with a cpp object file it is giving the error as follows:
$ dis6x.exe --all rbRsp_AngleEstimation.cpp.obj
Disassembly of rbRsp_AngleEstimation.cpp.obj…
George Mock said: I will file an entry and get you a link to it on Monday
I filed EXT_EP-11927 . You are welcome to follow it with that link.
Thanks and regards,
-George
Part Number: C6000-CGT Tool/software: The manual says that all v8.3.x versions of the c6000 compiler support C11, but I have the latest version as of today (8.3.13) and I can't select C11. It only goes as high as C99.
Tomas Nilefrost said: Should we try to create an additional forum post
No
Tomas Nilefrost said: can this be tracked through the same JIRA-ticket
Yes. In a part of the entry that you cannot see, I noted this problem probably occurs in compilers other…
Part Number: C6000-CGT Other Parts Discussed in Thread: C7000-CGT I write some C++ code using a lot of C++ template,use C6000-CGT or C7000-CGT compile too slow,takes 90s compiling one cpp file.
But when use ti-cgt-armllvm(tiarmclang),it works well,takes…