Zack, Thank you for your prompt response and your time. I understand your point, but I have a question regarding the mass production testing of your RF Evaluation Kits with matching circuit and antenna (Like CC1200EMK-420-470). Is output power testing…
Part Number: J784S4XEVM Hi,
we want to convert a RAW12 image (Bayer pattern) to YUV420 (NV12) on the TDA4. As far as we understood the VISS architecture we'll need the following modules: CFA (for demosaicing), Rgb2Yuv That also means it's okay to bypass…
Other Parts Discussed in Thread: CC1200 Hello,
I have some questions for the RF Layout Reference Design of CC1200 for 420-470MHz.
1. For the PA bias circuit, please let me know the purpose of R171, C173 and L171. Especially, I want to know the purpose…
Hello Brian,
I am attaching both captures, with 8ksps and 16ksps. We have 12 channels, and in this case we configured the channel 4 (fourth column) with MVDD as datashhet said, in ch4 MUX[2:0] = 011 means MVDD/4 in our case, 3.3/4.
The data is signed decimal…
Part Number: BQ40Z50-R1 Other Parts Discussed in Thread: GPCCHEM Hi
We have designed a 3S2P pack with Bq40Z50-r1 IC.
In this we have faced the following issue.
1.During the learning cycle the battery pack is not able to full charger to 12.6V when charging…
Hi Shreeharsha,
Here is the Foster ladder RC model for the TPS92624-Q1.
The second sheet titled "Thermal Model-Max Temp" allows you to enter the parameters for a transient power dissipation event.
20PWP_21262_TPS92624_RC_Network.xlsx
Regards…
Hello, Asha Bhandarkar
Asha Bhandarkar said: Can you clarify what version of TIDL and SDK you are using?
Our sdk version is 8.5.
Asha Bhandarkar said: Before integrating your model as a TIDL node, did you test the inference within the TIDL import/inference…
Part Number: BQ4050 Hi
Using CEDV mode, we found that at 5C rate, RSOC stops at 7% of EDV2. Only below 0.5C, RSOC can be discharge to 0%. Based on the above situation, the EDV0 point is fixed at 3V, then the RSOC jumps directly from 22% to 0 during 5C discharge…
I have attached a charge and discharge log for product 1. In the charge log you can see that the RSOC charges to 91% and then jumps up to 100% as soon as the charge termination current is detected. Also, during the charge, the remaining capacity increases…