Hello Eyal-san,
I apologize to bother you. I attach new logs which don't show error.
ap_conn_2018_06_25.xlsx is a log from uart_debug and AP_MODE_AP_20180625.txt is a log on the host (AM3352). They connected four STAs, and one of them is disconnected…
Hi Wyatt,
The previous overall charging current and voltage diagram is the voltage and the current passing through the adapter. The low-voltage battery is rated for 4.2V and 2A charging current.
The charging log is as follows:
kernel_log_1__2021_0526_073816…
Brad,
1.- Yes. Take a look at pictures RSTP_IDK_Test_1.jpg.txt, RSTP_IDK_Test_2.jpg.txt
2.- Take a look at picture RSTP_IDK_Test_1.jpg.txt.
I am plugging/unplugging both ports. You can see some traces in a post above with issue in eth2.
3.- The…
meminfo(1).txt
HI liu
Txt is the data counted to meminfo. The limit is run time is 550 and Memory leak begins.
During runtime, MemTotal remains unchanged, corresponding to a larger used in free m, but the process's physical memory does not gr…
Part Number: BQ76930 Hi,
We developed one BMS with BQ76930. And during 1C discharge test, we found a question when follow the steps:
1, Connect the BMS and a testing device in parallel with the battery.
2, Sync the local time with BMS and the testing…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: BQ34Z100-G1 , BQ76952 , BQ34Z100
Masters of TI,
I met a trouble,
1. My bq34z100-G1 is used with a 52V LFP battery (BMS).
2. The REGIN of bq34z100-G1 is connected to the REG2 (3.3V) of bq76952…