Other Parts Discussed in Thread: CC2400 Hello community,
I am programming highly demanding application from timing perspective using CC2400. I need to change between RX and TX states with minimum delay, i.e., with maximum speed allowed by hardware. My…
Other Parts Discussed in Thread: CC2400 , CC2543 Hi,
I am sure the blocking characteristics of the CC2400 and CC2543.
Is the blocking special quality of CC2543 excellent more than CC2400?
Best Regards,
hamada
Other Parts Discussed in Thread: CC2400 Hello,
don't know which forum I should use for my question, so I write here. Sorry if I'm wrong.
I'm using a device which uses a CC2400 and I try to send data from one device to another.
I know it is…
Other Parts Discussed in Thread: CC2400 For some reason I have to work with CC2400 which is not recommended for new designs. After reading the datasheet, I got two questions concerning the power supply for digital I/O.
1. I'm interfacing CC2400 with a…
Other Parts Discussed in Thread: CC2400 Hello,
I performed tests with a CC2400. I injected on its digital I/O a square signal which is half of the programmed bitrate. On the edges of the signal, I can identify a superposition of a sinusoid which frequency…
Other Parts Discussed in Thread: CC2400 , CC1100 , CC2500 I've been able to find the CC430s with the CC1100 integrated, but is there a CC430 with the CC2400 integrated? If not, are there plans to produce one any time soon?
Thx
Part Number: WL1837MOD Other Parts Discussed in Thread: CC2400 , , WL1837 Hi, w e are using the WL1837MOD in our Linux Armv7 based thermostat to scan for wireless BLE temperature sensors, which send a set of three advertisements (not connection oriented) every…
Other Parts Discussed in Thread: CC2591 , CC2430 , CC2400 , CC2530-CC2591EM I'm using the CC2400 with the CC2591 chip. I used the CC2430 CC2591 reference design since both the CC2400 and CC2430 have the same load matching. My problem is that I have to…
Other Parts Discussed in Thread: CC2400 , CC2500 I'd like to help my customer get clarity on a couple of specs on the CC2400. Please help clarify as soon as possible.
1) Image Channel Rejection @1Mbps is speced at 21dB
I assume this is the…
Part Number: CC2500 Other Parts Discussed in Thread: CC2400 , CC1310 , CC1120 We have a remote control customer who is looking for a solution with 1200BPS rate and - 120dbm receiving sensitivity. Does Ti have a corresponding solution.