Thanks for your response.
Yes, i was think in the baud rate, but i considered it does not mean a problem, because my SPI device work in 1 Mbps, and CC2544 in 2 Mbps (and the preamble, sync byte and CRC in the packet will not be the half of the packet…
Hi,
I already made some range tests using the two EM included in the DK,
after that I programmet to one of them my application (it did not work as I expected) then I opened the source code for the "per_test_cc2543em".
what happens is that in remote…
Other Parts Discussed in Thread: CC2544 , CC2543 I've been looking for a low power RF MCU with a very small form factor that runs at 3.3V and when I found the CC2544 it seemed like a good match. However, after reading the datasheet it seems like the CC2544…
Ionut,
I stumbled upon your post when looking for info on how to port the USB Software library from cc2511 to cc2544. How were you able to do it?
Thanks,
Ganesh
Hi Guys,
I am dealing with the same problem now, I changed the MODE nits in SmartRFStudio to meet the Auto mode 9-bit header as I see in the source code,
using GFSK 250 kbps 160 kHz and the same Synch word,
trying to catch the packets that transmitter…
Other Parts Discussed in Thread: CC2543 , CC2544 Hi,
I'm using IAR to program the chip. I have a C code used for programming CC2544, and now I want to do coding for CC2543 based on that. I changed the "device information" in the options (ALT+F7) of…
Other Parts Discussed in Thread: CC2544 When combining a TIVA C device with CC2544 connected via SPI can the DMA be used to transfer data?
Since the radio protocol and stack is running on the CC2544 we're trying to confirm that no CPU interaction is…
Other Parts Discussed in Thread: CC2591 , CC2543 , CC2544 Hello! What communication distance achieved CC2543-CC2544DK?, If we use "CC2543 + CC2591" and "CC2544 + CC2591": What communication distance is achieved? Best Regards