Part Number: CC3200 Other Parts Discussed in Thread: SYSCONFIG Hi team,
I have read https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wi-fi---internal/f/wi-fi---internal-forum/1233489/cc3220moda-wifi-at-command?tisearch=e2e-sitesearch&keymatch…
eventually, IT guy turn off wifi 6, make only wifi 4 available, and do some strange setting, which they don't understand why they make it works, now cc3200 can access server via 9120AX.
thanks.
Part Number: CC3200 Hello. When the CC3200 is acting as a Wi-Fi station. If the the simplelink device successfully connects to a desired access point but fails to find a DHCP server, then is there a possibility that it will assign itself a link local…
you can't delete it, but you should be able to re-write it without a token (it was supposed to be created with "public-write" flags that enables overwriting it (note that we use a "downgrade protection" mechanism so you can only use a newer SP - that…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , UNIFLASH What would be the best way to reset the target processor on a CC3200 Launchpad without reprogramming the flash ?
I've installed the latest Uniflash (8.5.0) and it seems like…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200SDK , UNIFLASH Hi team,
CCS:8.3.0
SDK:1.5.0,CC3200SDK_1.5.0\cc3200-sdk\example\p2p
Mobile phone model: Huawei Mate60
The program stopped in this while, the routine has not been changed…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: UNIFLASH , CC3200 , , CC3100 Hi there,
I've only seen this issue on E2E a couple times, with no actual resolution.
In attempting to connect to the CC3200 using UniFlash (3.4.1), I am getting…
Part Number: LAUNCHCC3235MOD Other Parts Discussed in Thread: CC3200 , SYSCONFIG
How would I adapt some cc3200 code that looks like:
//AESCrypt(uiConfig,uiKeySize,puiKey1,puiData,puiResult,uiDataLength,uiIV);
AESCryptuc(uiConfig,uiKeySize,puiKey1,&(acmsg…
Part Number: CC3200-LAUNCHXL Other Parts Discussed in Thread: CC3200 , CC3200SDK I am attempting to setup the CC3200 Launchpad on my second laptop and unfortunately I am getting driver problems. More specifically "Windows cannot load the device driver for…
Part Number: CC3220S Other Parts Discussed in Thread: CC3200 Hello everyone
I am using the custom board my all example are working properly when i use IC (CC3200) everything is working and wifi is also working. But when i change IC to CC3220S on custom…