Part Number: CCSTUDIO-C2000 Hi Experts,
Could you please teach me if C2000 Hex Utility generates .m00 .m01 and .x00 .x01? According to www.ti.com/lit/spru513, they seem --motorola=1,2, or3 -m1,2,or 3 Motorola-S1, 2 or 3 and --tektronix -x Tektronix…
Part Number: CCSTUDIO-C2000 Hi there,
I'm using CCS for the C2000 F28388D MCU, and I have a workspace with projects for the different CPU cores. I have defined several Debug Configurations, using different options and different project outputs for the…
Part Number: CCSTUDIO-C2000
hi,experts
My CCS version is Version: 11.2.0.00007.
Now I am encountering one problem: in debug mode, I cannot find "back" or "forward" button icon.
but in edit mode, these button icon is still there.
it's very…
Part Number: CCSTUDIO-C2000 Hi Experts,
I am asking for my customer.
Customers are evaluating STM32G474 and C2000, care about the development tools Keil and CCS.
You can see the below action, they can lookup the address of the variable without JTAG…
Part Number: CCSTUDIO-C2000 Hi team,
Customer is surveying whether it is possible to get the compiling time stamp in CCS?
For example they could define some like #Define TimeStamp Getting_Compling_Time. Then CCS would recognize this key word and return…
Part Number: CCSTUDIO-C2000 Hello, I'm working on a project where i'm trying to implement structure packing. CCS is returning error for this. Kindly let me know the solution for this problem. Let me know if any other info is required from myside.
I…
Part Number: CCSTUDIO-C2000 I got a compile error with CCSv11 for my old C2000 project (used to use CCSv5.3).
I saw this thread e2e.ti.com/.../2046257 talking about the same error "Product XDAIS v0.0 is not currently installed and no compatible version…
Part Number: CCSTUDIO-C2000 Hello,
I am currently working on a project involving a TMS320 Micro-controller and our team has to provide evidence to the customer that our code complies to the MISRA-C:2004 "Required" rule set.
We use the analysis tool…
Part Number: CCSTUDIO Other Parts Discussed in Thread: C2000WARE Hello,
I recently installed C2000 ware version 4.01.00.00 and CCS version 12.1.0. Then I imported a project created by another colleague and I get this error:
Product c2000ware_software_package…
Mark Philip Felipe said: "Do you have the debugger memory map configured the same for both CCSv5 and CCSv10.4?" Do you mean "Debug Configurations"=>"Target" => "2809 Flash Settings" ? If so yes they are set up the same.
Actually, I am referring to:…