Part Number: CD4013B Hi team
There are two questions. Could you support these?
Could you tell V_IL(max) at VDD = 3V?
They want to set Q1 to Low when the VDD is turned on. During this time, there are no signals in CLOCK1 pin. They want to prevent…
Part Number: CD4013B Other Parts Discussed in Thread: SN74LVC1G175
Tool/software:
Hi, I'm currently developing a circuit similar to the one found in TI's application note SCEA048–April 2017 (Push-Button circuit) using the CD4013B, since I'm operating…
Part Number: CD4013B Dear Technical Support, attached is CD4013B datasheet and P.4 of the related datasheet, the circled area of P.4 shows that the " Clock Input Frequency " related data, and it listed the MIN. & TYP. data values,
but not listed the…
Part Number: CD4013B Other Parts Discussed in Thread: SN74LS279A , , SN74LS74A , SN74LVC2G02 Tool/software: I am looking for an SR latch with non-inverting inputs (set, reset) and both inverted and non-inverted outputs available. CD4013B meets my requirement…
Part Number: CD4013B Tool/software: Hi team, When the output pin is Low, negative voltage is generated by the load that leads. At that time, current flows from the output pin, so is there any spec for the maximum current? BR, Kengo.
Part Number: CD4013B-MIL Other Parts Discussed in Thread: SN54LVC74A-SP , CD4040B-MIL , CD4047B-MIL , CD4070B-MIL , CD4081B-MIL , SN54LS393-SP , SN54LVCH244A-SP , SN54LS08-SP Tool/software: We are looking for Radiation Tolerance value for the above part…
Part Number: CD4013B Hello.
I need a help with the PWR package footprint land pattern details.
The mechanical drawing does not include these details.
This is the pdf file for TSSOP PW14 package (see attached).
https://www.ti.com/lit/ml/mpds360…
Part Number: CD4013B Hi Team, Our customer reported a possible discrepancy on the CD4013B datasheet first page. They tried to simulate it and it does not work properly. Below is their simulation circuit. According to them, if the circuit is correct, then…