Part Number: CD4043B Hi,
Sofarsolar is trying to use the CD4043BDWR. They need the ESD information for this part.
Since it is very old device, the datasheet doesn’t contain this information.
Would you please share it?
Thanks.
Part Number: CD4043B Hello Team, is there any suggested way (e.g. external circuitry) so that the output state after powerup can be defined? From the other related post, I understand that no fixed state can be assured with this IC alone. Regards, Dav…
Part Number: CD4043B Hi Team,
may we ask if the truth table of these two are functionally the same? our CD4043B truth table is below, can the CD4043 truth table fully replace the ocmpetitor version? because after replaceing it with the CD4043B, the…
Part Number: CD4043B Tool/software: Hi experts,
I have a question regarding the output propagation time.
The datasheet has “Max value for tPLH = 300ns under VDD=5V”. Under VDD=3.3V, what would be the MAX value for tPLH?
In actual measurements…
Part Number: CD4043B Hello TI, I was simulating the CD4043B (S/R latch) using TINA and I found an issue. When S=0 and R=0 the output (Q) seems to be toggling between logic '1' and logic '0' whenever the enable pin is toggling. So when enable is high,…
Part Number: CD4043B Other Parts Discussed in Thread: SN74AUP2G02 , SN74AHC02 Tool/software: Hi experts,
I would like to ask you about CD4043B.
I saw there are data at VDD=5,10,15V on datasheet.
but would you share the threshold of ENABLE high…
Part Number: CD4043B-MIL Other Parts Discussed in Thread: SN74LVC1G98 , SN74LVC2G02 , CD4043B , SN74LVC2G74-Q1 Is there a single channel small RS Latch out there? I just need one bit with no clock. Press one button, the output goes high, press the other…
Part Number: CD4043B Other Parts Discussed in Thread: SN74LS279A Dear team,
Do we have new device to replace CD4043B? CD4043B have 4 channels, 16pin. Currently the customer only needs 3 channels, and they hope smaller package.
I didn't find other…
Part Number: CD4043B Team,
Can CD4043BD(W) or CD4044BD(W) be safely operated with Vdd=3.3V and input levels up to ~3.3V (HIGH) o ver the entire temperature range?
Use case: supply voltage is Vdd = 3.3V our logic levels are 0V (LOW ) and 3.3V (HIGH…
Part Number: CD4043B Hello,
I considering thermal analysis of circuit board using CD4043BD.
I would like to confirm thermal impedance data of CD4043BD.
(Thermal impedance of junction to ambient and junction to board)
* The data sheet of CD4043B…