Part Number: CD4046B Hi, Support team!!
I am using CD4046B with Vdd = 10V, R1 = 300k, C1 = 50p, VCOn = 0V. So we check the oscillation frequency of the VCO. And when I checked the data sheet, I found the following statement.
There is no description…
Part Number: CD4046B Hi, Customers want to check the impedance of each pin. However, because the data sheet is old, the description of each pin and I/O information are not described. https://www.ti.com/lit/ds/symlink/cd4046b.pdf Could you tell me the pin…
I cannot observe the difference in my diagram and the Figure 10 on the data sheet of CD4046B. The figure 10 is behaving exactly as my diagram so the states is right between 2 and 3 it cannot go high as in Figure 10 of data sheet.
Part Number: CD4046B Hello! I am in trouble of simulating about PLL. I haven't sought CD4046 Spice model from TI official website. How can I get CD4046 Spice model. Expect for yor help. Thank you!
Part Number: CD4046B Other Parts Discussed in Thread: LM331 Hi,
Would be possible to achieve something like this with cd4046b ?
I'm trying to achieve the Buchla synthesizer style Phase lock circuit, which locks the main synthesizer VCO to an external…
Part Number: CD4046B Hi,
I designed an FSK system with a 555 timer as a modulator and CD4046B for demodulation.
The system sends signals at around 45kHz for binary '1' and around 25kHz for binary '0'.
When I send information over the…
Part Number: CD4046B Other Parts Discussed in Thread: SN74LV4046A Hi Team,
I am looking for a PLL that accepts a input of 210Hz. I need the output to be 5 times the input (i.e 1050Hz).
I found CD4046B, can you please verify that the CD4046B is suitable…
Part Number: CD4046B Greetings! I aim to build a grid tie inverter. So far, i have generated a pure sine wave of 50Hz (grid frequency) but there is a phase difference between grid and inverter output. As I know phase lock loop PLL is a good way of eliminating…
Part Number: CD4046B Hi Team,
My Customer wanted to know which equation for Frequency Capture Range (2Fc) is correct or why the datasheet vs application note equation is different? From the datasheet of CD4046B (page 3-125) equation for 2fc is having a multiplier…
Part Number: CD4046B Hi
According to datasheet, there are some limitation of the external component as below.
If the component such as C1 is smaller than above range (e.g. In case of 100pF<C1 @VDD>5V or 50pF<C1 @VCC>10V)what is it concerned? (What is…