Part Number: CD4053B-Q1 Hi Expert,
We noticed that the truth table of CD4053B-Q1 in datasheet page 16 is confusing.
No matter the high or low of A, B, C, the ON CHANNEL(s) are all ay or by or cy?
Could you help us to confirm it?
Thanks a lot for…
Hi Baron,
With below pin out of CD4053B :
To measure Ax OR Ay to Ay cross talk (pin 14 to pin 13, switch closed on ax), the channel input and output is connected to the network analyzer as below.
The equation used to generate the plot is:
Crosstalk (dB…
Part Number: CD4053B Other Parts Discussed in Thread: SN74LV4053A Hello E2E,
Our customer has plan to use the CD4053B on 3.3V single power. This device's minimum power supply voltage is written 3V(Vdd-Vss) in datasheet. However, data with 3V power is…
Part Number: CD4053B-MIL I'm trying to purchase PN CD4053BF3A and your website states there is stock at Rochester. After contacting Rochester I found the parts are marked as Harris semiconductor with PN CD4053BF/3. I cannot find any information as to…
Part Number: CD4053B Dear all,
one of my AA has used the CD4053B in several projects, but some boards returns from the field showing high current absorption of the device.
I have schematic and analisys report, but I need to share it by email.
Please provide…
Part Number: CD4053B Other Parts Discussed in Thread: TS12A12511 Hello,
I have a question on the CD4053B part - I see that it uses the voltages, Vee (Negative power input) and Vss (Ground). In what circumstance would Vee be used?
Thanks,
Andrea
Part Number: CD4053B Tool/software: Code Composer Studio if the power supply to CD4053 is VDD=5.5V VSS=0V VEE=-5.5V, can I use digital control signal at 3.3V (MCU IO) ?
Plus, is there a similar switch ic to CD4053 fitting to the above voltage setup, but…
Part Number: CD4053B Other Parts Discussed in Thread: SN74CBTLV3257 E2E,
Is CD4053B output condition in high impedance when the device is not power supplied with any INH pin position?
I looked for relevant documentation regarding this condition in the…
Part Number: CD4051B Other Parts Discussed in Thread: CD4053B , CD4052B , Hi all Would you mind if we ask CD4051B, CD4052B and CD4053B? <Question1> RDS is 470ohm(typ) upto 1050ohm(max) in case of 25C. So, if the device'S RDS is 1050ohm@25C, in case of…
Part Number: CD4052B Hi all Would you mind if we ask CD4051B , CD4052B and CD4053B ? How much is the input leakage current with Vcc=3.3V, 5.0V and Ta=100C? On the datasheet P7 shows, it shows "OFF Channel Leakage Current Channel OFF (Max) or ALL Channels…