Part Number: CD4067B What is the maximimum split supply voltage I can use on the CD4067B? According to the note below it says 24V which contradicts the recommended and maximum operating conditions. Which is right?
Also, assuming 18V is recommended…
Part Number: CD4067B Clemens, Related to the following E2E thread, my customer has a further question. CD4067B: Any tr/tf limitation for control input PINs? - Switches & multiplexers forum - Switches & multiplexers - TI E2E support forums They will use…
Part Number: CD4067B Other Parts Discussed in Thread: CD4013B , Hello, My customer would like to add some CR filter to eliminate noise for control input A, B, C and D pins. Are there any tr/tf limitation for the control inputs? Or the tr/tf could be slower…
Part Number: CD4067B Tool/software: The original datsheet (probably pre 2003) is listing following values for Vil and Vih:
The new revision datasheet however is listing this:
What are the correct Vil values for the CD4067B?
Is the old sheet…
Part Number: CD4067B Tool/software: Hello,
I am using an CD4067BPWR Chip on a current Project. When adressing Line 10 with the following Settings.
Pin A = 0.05 V
Pin B = 12 V
Pin C = 0.01 V
Pin D = 12 V
Inhibit = 0.00 V…
Part Number: CD4067B Tool/software: I'm trying to see I am thinking of this properly. I have a 17 position rotary switch (16 points and a common) and I was wondering if I could use the 16-channels of the CD4067 to let a computer know based on the position…
Part Number: CD4067B In the CD4067B datasheet (and in the J (R-GDIP-T**) mechanical drawing), there are Narrow and Wide dimensions given for the J package. The "C" dimension is different between the Narrow and Wide package. Does the CD4067B package have…
Part Number: CD4067B Other Parts Discussed in Thread: ADS8684 , LM2904 Hi TI,
In our application, we're using a series of stacked multiplexers (CD4067B) to multiplex DC voltage from 320 LEDs down to one read from an ADS8684 ADC. I've attached a simplified…
Part Number: CD4067B Hello
I would like implement in my design a MUX CD4067BM, unfortunately i can't find data in the data sheet :
A. On the chip exist pin # 15 with name INHIBIT - what for that pin and how i work with him?
B. i would like pass…
Part Number: CD4067B Other Parts Discussed in Thread: MSP430F6736 , MUX506 Hi team,
I am working with CD4067B on a project. I am sending the select signals A,B,C,D and the inhibit signal using msp430f6736. However, I am unable to switch the input lines…