Part Number: CD4069UB Hi Team,
As per datasheet it shows lead finish for MPN CD4069UBPWR "NiPdAu | Sn". I also tried to find it by using path "TI.com > Quality & Reliability > Material Content Search " but not getting proper information attached Link…
Part Number: CD4069UB Hi dears
I'm looking for CD4069's Altium designer library (Just for Schematic and footprint not for simulation with altium), can you help me please?
I downloaded the TI Altium libraries but i cant find CD4069 in the libraries…
Part Number: CD4069UB We are having issues with this IC and in some boards it's locked on low level output when input is also low.
Power supply is 3.31 volts.
There is quite a few with this problem.
Could TI tell me something about this lot (IC…
Part Number: CD4069UB Hi team
My customer considers using CD4069UBPWR(TSSOP package). However, ±1kV HBM is required for their application.
Could you please confirm if CD4069UBPWR is guaranteed to meet ±1kV HBM?
Please let me know if you have any…
Thanks a lot
In gate library i find CD4069 and by the path: "right click >edit component > show hide pins" i see the source pins of the component so i connect source pins with a battery and ground, so I give my answer.
Thank you
Hi Mohammad,
TI does not have spice model for this specific part. But you might want to check this database to find similar parts that might have model that might potentially you can use for your simulation.
webench.ti.com/.../
If you can't…
Part Number: CD4069UB Hi Team
In CD4069UBNSR’s datasheet, ESD rating is ±500V for HBM.
My customer wonders if TI have actual tested value for CD4069UBNSR for over ±1kV HBM?
±1kV HBM is customer’s main concern to adopt CD4069UBNSR.
Please let me…
Part Number: CD4069UB Dear Technical Support Team,
The absolute MAX of VIN on datasheet shows 0.5V(MAX) and -0.5 to Vdd(MIN) below.
I think that this is typo and "Vdd+0.5V(MAX)" and -0.5(MIN) correctly.
If it is typo, could you fix it ?
…
Part Number: CD4069UB Other Parts Discussed in Thread: CD40109B i needed to step up the 3.3-volt logic to more than 8 volts. we have CD4069UB ic available with us. when i saw datasheet i could see that by using VDD at 10 or 15 volts. the input PWM can…