Part Number: CD4093B Tool/software: Hi my understanding from the Texas forum is that IBis model is not available for CD4093 & CD 4034 but I want ro run Signal integrity, is there any close approximate model that I can substitute as I only want the IO…
Part Number: CD4093B-MIL Other Parts Discussed in Thread: CD4093B , TLV803E I have configured an RS Filp-flop with two of the NAND gates in the CD4093B package. When the power is applied, both inputs are biased up to Vcc (11.4V) through 100k resistors. …
Part Number: CD4093B-MIL Other Parts Discussed in Thread: CD4093B , CD4044B , TL7733B , TPS3710 , TL7700-SEP Attached, is our circuit; a well-known RS Flip-flop configured from two of the NAND gates within a CD4093B. for some unknown reason (and luckily),…
Part Number: CD4093B I'm running into a problem with the PSpice model that I downloaded from the product page for the CD4093B.
I'll be the first to admit I'm not an expert when it comes to reading model syntax, but it appears to me that the subcircuit…
Part Number: CD4093B Hi,
I have trouble to correctly set the CD4093 initial status. I use CD4093B to implement battery cutoff and latch function. See my schematic below.
However, when I test the circuit, After startup (at Vin=10V), I don't get what I…
Part Number: CD4093B I want to simulate a missing pulse detector with CD4093B in PSpice for TI. I need to use a Schottky Diode from Toschiba in my schematic. The corresponding PSpice Modell was found on Toshibas web site and copied on my PC. How I can…
Part Number: CD4093B-MIL Other Parts Discussed in Thread: UC1705 CD4093 output is fed to a npn-pnp based totem pole circuit to drive a Mosfet. A resistor of 1kohm is provided in between the cd4093output & base of the totem pole circuit. Now observed that…
Part Number: CD4093B Part Number Differences
Between CD4093BE and CD4093BEE4 what additional suffix E4 means for CD4093BE
Between CD4093BF3 and CD4093BF what suffix 3 means for CD4093BF