Part Number: CD4093B Hi team,
The customer is using CD4093B. On his boards, many CD4093B devices are hot serious. And the supply voltage of
CS4093B is pulled low. The customer's schematic is in the attach. VA+ is 15V.
Q1: Can D pin, H pin and E pin…
Part Number: CD4093B Hii,
We are from India. We have buy CD4093BE from your TI store . Previously we where using HEF4093BE . but now PHILIPS part is discontinue .So we have ordered equivalent of that CD4093 BE. But that same part is not working in our…
Part Number: CD4093B Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hi,
a simplest oscillator with :
1 NAND trigger 4017( macro in TINA)
1 R (22K)
1C (100nF) gives to me stange results in transient mode when connect as…
Part Number: CD4093B Hi, Team,
I have one question about CD4093B from customer.
Customer found that in their design for CD4093B, pin 4 will be damaged and short to pin 7. And they found that the pulse current through pin 4 will be 36.8mA peak, time is…
The specification "V IL(max) = 1.5 V" means that all input voltages up to 1.5 V are guaranted to be interpreted as low. Similarly, "V IH(min) = 3.5 V" means that all input voltages down to 3.5 V are guaranted to be interpreted as high…
Other Parts Discussed in Thread: CD4093B-Q1 Hi,
what is the Maximum allowed junction temperature of the CD4093B-Q1 during Operation?
I cannot find it in the datasheet.
many thanks,
Katharina
Part Number: CD4093B Hello,
Regarding to threshold voltage on CD4093BE, my customer is asking a question.
(datasheet page2)
(Question)
(1) They are understanding about input test condition (Vin) (a,b) with following diagram.
Their understanding is…
Hi,
I use CD4093B. The same signal "RESET" (capacitor charge at power ON) arrive on the inputs of two input gates
Is the same positive Trigger Threshold Voltage for all the gate in a package ?
Is both output on the gate switching at the same…