Part Number: CD4541B Other Parts Discussed in Thread: TPL5110 Tool/software: Hello,
I am considering the use of the CD4541B timer IC to implement a time delay from 0 to 10 minutes in a relay-based system.
The behavior I need is:
While the coil …
Part Number: CD4541B Tool/software: Please refer the attached document. We would require support to find out the presence of dechlorane and UV328 substances in the components listed in the document.
Preliminary analysis has been done by checking the…
Part Number: CD4541B Tool/software: Hi,
I am using CD4541 in single transition mode with auto reset disable, Q high after reset and VDD is 3.3V. The below is the circuit diagram.
The current consumption by the IC is 260uA, where as the datasheet…
Part Number: CD4541B Hello,
For a while now we have had a product that uses two CD4541 to set a clock period and pulse width. This is an old product that is predominately on through hole technology and I am currently updating it to surface mount. My…
Part Number: CD4541B This part looks great for my application. It is able to be retriggered and it has clock frequency division. My biggest concern is that in the data sheet under features it states that the oscillator frequency range is DC to 100kHz…
Part Number: CD4541B Other Parts Discussed in Thread: SN74HC4060 , CD74HC4060 We have implemented the component but we have some problems with it during our tests.
Configuration of the CD4541B :
Between pin 1 and 2: a Resistor and a capacitor R=56Kohm…
Part Number: CD4541B Hello,
I am trying to simulate the CD4541 timer on LTSPICE.
I acctually use a sborka library but this library dosn't work well.
Someone has a spice model of CD4541 or equivalent ? I urgently need it.
You can found below my…
Part Number: CD4541B Hell, Everything is in the title.
I'm working for very sensitive industry. I need to argue why in product I designed I have to introduce an x2 factor in the value of Rtc to get the good timing value.
For instance to get 25s with…