Part Number: CD74HC4051 Tool/software:
Hello,
For the CD74HC4051's three select inputs, what are the IIL and IIH currents?
I need to do some fan-in and fan-out calculations and am checking the driver can connect to multiple CD74HC4051s.
thank…
Part Number: CD74HC4051 Hi team,
My customer is using CD74HC4051M96 in traction inverter and meet damaged issue.
Pin13 and Pin14 are short to VEE.
Yellow means pin16. Blue means PIN14. Red means PIN13.
Q1: Though in datasheet, input signal…
Part Number: CD74HC4051-EP HI,
Our customer is considering the EP version because the standard HC4051 has low ESD immunity.
Is this device the same DIE as the standard product, with only the testing being different?
Or is it a product with a different…
Part Number: CD74HC4051 For TI part numbers CD74HC4051 I am requesting the following information.
Tin plating process (i.e., electroplate, immersion, hot dip), tin thickness (microinches), is tin annealed (yes/no), material underneath tin plating (copper…
Part Number: CD74HC4051 Tool/software: Hi Experts,
This is Skylar responsible for GREE.
GREE wants to know that if they have unused input pin of CD74HC4051, what do you recommend for it, floating it, pullup or pulldown? Thanks.
BR,
Skylar
Part Number: CD74HC4051 Tool/software: Hello,
Does the voltage on the channel input [A7, A6,...A0] has a impact on the quiescent Current of the 74HC4051 when the chip is disable (/E=1)?
For information, on my board, VCC=3.3V, VEE=GND and A7..A0…
Part Number: CD74HC4051-Q1 Hi team,
I would like to understand the maximum rating of IO pin input voltage. I don't find a specific withstand voltage for IO pins. Should we refer to the input/output clamp current? If customer can ensure input current…
Part Number: CD74HC4051 Hi team,
My customer is using CD74HC4051 for measurement of Battery pack's voltage.
Battery pack's max voltage is 1000V and customer use several resistors to divide it to 2V then to CD74HC4051.
Usually, customer will not…
Part Number: CD74HC4051 Tool/software: Experts,
Customer is running into issue with another vendor and wants to try using TI. Needs the data of expected resistance between VEE(negative voltage bias) and GND.
Can you also share the same data for…
Part Number: CD74HC4051 Tool/software: We are having some TI VPN CD74HC4051M fail during our preliminary card test. We are seeing about 0.5 V difference between the channel In/Out pins 1, 2, 4, 5, 12, 13, 14, and 15 to ground. I suspect there was a die…