Part Number: CD74HC4052 Hi Team,
Customer has quick question.
below graph was testing EN (pin6) at 5ms condition
S0 & S1 were fixed at LOW
Output AN depends on EN LOW (on) ,HIGH (off)
2. Below graph was testing EN at 50us condition
S0 & S1 were…
I doubt that 4.5 V would be much of a problem. But the datasheet does not guarantee it.
Anyway, the CD74HC4052 would not allow more than 10.0 V. But the TMXU6209 does what you want.
Part Number: CD74HC4052 Other Parts Discussed in Thread: TS3A5017 Hi Team
My customer wants to use the 74HC4052 as a I2C mux and needs the switch characterization data at 3.3v. Do we have this data available?
Thanks
Jeff Coletti
Part Number: CD74HC4052 Other Parts Discussed in Thread: TINA-TI , TS3A5017 , TS3A5017-Q1 , Tool/software: TINA-TI or Spice Models Dear TI Team
We required TINA simulation file of CD74HC4052PWR for SWD signals muxing would you like to provide TINA simulation…
From what information I've been able to find, AHD is just standard composite video with higher frequencies, typically 40 MHz, depending on the resolution.
I suspect that your oscilloscope triggered on the vertical/horizontal blanking intervals.
Video…
Part Number: CD74HC4052 Hi, All:
As the title, if CL is zero, I think total capacitance is Ci(Switch input capacitance) + Co (Common output capacitance)
Am I right??
Part Number: CD74HC4052 Other Parts Discussed in Thread: MUX36S16 I have one question regarding the test measurement of our part:
CD74HC4052PW in TSSOP16
The following parameter is used in the data sheet "Iz = Switch ON / OFF Leakage Current" as follows…
Part Number: CD74HC4052 e2e,
Please provide the Rdson of CD74HC4052 device with Vcc = 3.3 V. The datasheet only shows Rdson with Vcc = 4.5 V.
Thank you,
Adam
Other Parts Discussed in Thread: CD74HC4052 Hello,
The enclosed schematic (please see below) is part of a CAN Bus tester. The tester is powered from a USB port. As you can see in the schematic, the can bus signals drives a MUX (CD74HC4052) via a 50K resistor…