Part Number: CD74HC74 Dear Technical Support, Good day!
SFO TECHNOLOGIES reported that CD74HC74M96 does not respond to the input signal.
The problem was resolved after replacement and the board operation function normally
Please provide guidance…
Part Number: CD74HC74 Dear Technical Support, Good day! Customer reported that CD74HC74M96 does not respond to the input signal.
The problem was resolved after replacement and the board operation function normally
Please provide guidance for proper…
Part Number: CD74HC74 Other Parts Discussed in Thread: SN74LVC1G80 I have a query regarding a possible failure mode of the CD74HC74M D-Type Flip-Flop.
It is proposed to use the flip-flop on the output of a 16MHz Crystal Oscillator to reduce the clock…
Part Number: CD74HC74 Hi, Good day. Our customer is looking for the ESD information (HBM & CDM) for CD74HC74. Can you please help us? Thank you. Regards, Cedrick
Part Number: CD74HC74 Dears
We are using a CD74HC74M96 D flip-flop chip. The wiring diagram is as follows.
After the chip is powered on, the ~R and ~S pins are both pulled high. According to the truth table, Q should output 0V. But after I touch the…
Hey Scott,
I was able to pull some data for you -- here's a few typical waveforms for the CD74HC74.
All tests were performed at 25C on a 50pF load
Figure 1 - 6V output
Figure 2 - 6V output, zoomed rising edge
Figure 3 - 5V output
…
Part Number: CD74HC74
Hi every one,
I have been designing complex digital ASICs for the last 20 years. I developed design techniques and devices that could be used at advantage in 74 / 4000 like devices, allowing for
FULLY SYNCHRONOUS DESIGNS (FSD…
Other Parts Discussed in Thread: SN74HC74-EP , CD74HC74 , SN74HC74 Hello,
Im working on implementing a replacement for a previous flip flop I had in my design that went obsolete. It looks like I have a choice between either the CD74HC74 and the SN74HC74…
Hi Patrick,
For the second question, as the below TIDA-00961 guild book said, that if you run the project in open loop, you should make sure that INCR_BUILD is set to 1, DEMO_MODE is set to 0, and DC_CHECK is set to 1 in the pfc2philtrmttpl_settings…