Part Number: CSD16407Q5 Hello TI team,
We are using CSD16507Q5 in our design and are considering adding a heatsink between the package top surface and the heatsink.
We would like to ask about the mechanical limitation of the package during…
Part Number: CSD16407Q5 Hi Expert,
The customer sees the CSD16407Q5 is damage on their applicant.
The user case is Oring-Fet of power supply .
The engineer need TI to confirm the question below:
Pls check whether CSD16407Q5 is capable to…
Part Number: CSD16407Q5 Hi Expert,
The customer need to know the ESD rating of CSD16407Q5 DS.
Pls advice.
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E…
Part Number: CSD16407Q5
Hello E2E team
I am Customer Quality Engineer for Rochester Electronics I am trying to clarify an date code issue for our customer. The customer is questioning if this is actually a date-code 1823 as you can see in there…
Part Number: TPS24720 Other Parts Discussed in Thread: CSD16407Q5
Hi Team,
Issue found:
Board A is working normally in the chassis. Board B(with hot swap TPS24720) plug in cause board A to restart.
TPS24720 GATE voltage drop is detected
Connecting…
HI,Terry :
Thanks for your feedback, you can finally start discussing this issue. First, the ACP pin is derived from the 19V voltage (used by the Charger). When the DSG protection test is performed, the 19V voltage has been cut off, and the 19V voltage…
Kanemaru san,
Thank you for your question.
Unfortunately this is not a curve that we provide with this device.
However I can provide a discrete part number that would have very similar transient thermal impedance performance and could be used with…
Part Number: TDA4APE-Q1 Hi, Different line impedance mentioned for PCIe ref clock. Below near Clock generator, it says 100 ohms: but near PCIe connector it says, 85 ohms: PROC184E2(002)_SCH.pdf and for PCIe data lines it says 85 ohms, But some references…
Hi Booby,
Thans for your info.
May I know whether the level translation working if we give the 3.3V to output sides? because by default 3.3V is connected to the input side and now we planned to connect the 3.3V at output side.
PROC141E4(001)_SCH…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…